Part Number: DRV8308EVM Other Parts Discussed in Thread: DRV8308 i use the controller DRV8308 (evaluation kit) to control and drive 3 phase BLDC blower. i have a problem when i want to reach the maximum RPM of the blower. when i increase the pwm duty cycle…
Hello Adam
I don't understand your answer.
The above question looks like i has not yet been answered and my question is not just related but the same problem.
So why should I ask a related question then?
-------
Meanwhile I found a solution:
It looks…
Part Number: DRV8308EVM Other Parts Discussed in Thread: DRV8308 , MSP430G2553 Hi,
I'm i'm using DRV8308-EVM to evaluate scroll compressor.
Can you please let me know how to program MSP430 in DRV8308-EVM? Can I use Micro USB cable (through J3 Micro…
Part Number: DRV8308EVM Other Parts Discussed in Thread: DRV8308 Hi,
Why strong pullup resistor (R5, 390E) used for FGOUT signal in DRV8308EVM board? I went through the datasheet of DRV8308 and it never recommended any strong up resistor for FGOUT?
Siv…
Part Number: DRV8308EVM when motor running using PWM mode setting and try switching to register mode and write configuration ,the motor stopped . i can't understand what happen ? and how to write registers and control speed
Part Number: DRV8308EVM When I start this up the serial options are greyed out and not selectable. At the bottom I get a continuous status of ' connecting to TI cloud agent ...' Is that supposed to resolve somehow? Does it need a firewall exception…
Part Number: DRV8308EVM When I download this software and the web based app appears, connecting the USB cable to the EVM board installed the USB drivers. The green LED V3P3 illuminates, however its continues to say connecting... on the status bar. I have…
Part Number: DRV8308EVM Other Parts Discussed in Thread: DRV8303 All done as administrator on a Win 10 machine.
First, when installing (from slvc552f.zip) , installer complains that no valid "GUI Composer Runtime" is available. I tried the choice…
Part Number: DRV8308EVM Tool/software: TI C/C++ Compiler i am using drv8308evm software to spin bldc motor when i am try to operate motor at clock frequency mode at high speed rotated when motor is heat
mode120= 3970;
speed=4000;
fclk=1.2khz
using hall_u…
Part Number: DRV8308EVM Hi,
I'm using the DRV8308EVM with the supplied motor and GUI version 1.0.1 and cannot get Clock Frequency Mode to work at all. PWM mode using the speed control register works fine. Is there a list of all the register settings needed…