Part Number: DRV8311 Hi Team
do we have any other motor driver solution only HW config like DRV8311H but MCU no need to send PWM singal.
MCU only need to control orientation?
BRs
Brian
Part Number: DRV8311 Hi Team,
There are couples of questions regarding DRV8311, could you please share your insights regarding the questions? Thanks.
If the LDO is unused, we should just connect the capacitor 4.7uF between AVDD and AGND, right?…
Part Number: DRV8311 I have an application where we have four cameras and to deal with rain it was chosen to use spinning lenses. One of the motor drivers in consideration is the DRV8311. In our scenario the rotation speed has to be just above a threshold…
Part Number: DRV8311
Datasheet states SDO output current is 1 micro ampere. This is physically impossible given the actual maximum output data rate of 10 MHz. (DRV8311 SLVSFN2B – SEPTEMBER 2021 – REVISED FEBRUARY 2022).
We have reached out to…
Part Number: DRV8311 Hi,
We use DRV8311 for the motor driver with the 3 PWM mode, and now, we test the board that the no-load current is High(The input current is more than 0.14A), please check our schematic diagram that if there are any error, thanks…
Part Number: DRV8311 Tool/software: Hi,
We use the DRV8311 for our BLDC drvier, and now, the SOC pin is the below waveform and there are no c omplete sine wave, but the motor spec. is normal,
So please advise if this wavform is right or not? thanks…
Part Number: DRV8311 Other Parts Discussed in Thread: DRV8376 Hi Sir,
My customer is currently evaluating the DRV8311H (Hardware Control) for my project. I would like to inquire if it is possible to configure the Over-Current Protection (OCP) threshold…