Ok, I posted the announcement here , but not sure if anyone will really see it hidden away.
For those of you who have a DRV8312-C2-KIT (or once you purchase the new 60A DRV8301-HC-C2-KIT) I'd love to hear your feedback and see some videos of how fast…
Sidharth,
1. DT4260-24-055-04 BLDC motor comes with hall sensor. You will have to choose another motor if you are looking for encoder inetrface.
2. The Insta-spin lab projects are aimed mainly for sensor-less foc control and I think one/two lab exercises…
With the DRV8312-C2-KIT
It doesn't provide enough current, but for initial evaluation I don't think your motor will draw that, I'm sure that's under some sort of load, correct?
There is a GUI available for a new technique called InstaSPIN-BLDC …
I'm making PMSM motor driver with drv8312 kit, and I made it almost, except of motion profile. by using CLA, to do paralel processing, I'm trying to program real time motion profile generator in CLA. so, when I calculate the motion profile with floating…
Other Parts Discussed in Thread: TMS320F28027 , DRV8412 , DRV8312 Hello, I recently received my TMDXIDK3359 and am very enthusiastic about the possibilities! I want to perform some basic motor control (BLDC) proof of concepts via the Piccolo controller…
Other Parts Discussed in Thread: CONTROLSUITE , UNIFLASH , DRV8312 , INSTASPIN-BLDC I am doing the procedures described in file CCSv4HowToFlashcontrolCARDS.txt from the USB-flash card attached to the developer's DRV8412-C2 kit.
A bunch of errors occur…
Other Parts Discussed in Thread: DRV8301 , DRV8312 HI, I'm running my custom motor using the DRV8301 kit with the RM46 controlcard using the instaspin software project. I've done this with a F28035 controlcard on a DRV8312 driver board, so I know that…
Floating point is really about ease of use. There are some operations that are slightly faster, but in an overall system you won't see a huge gain.
The DRV8312-C2-KIT ships with the Isolated F28035 controlCARD, but the code is dual built to also support…
Thanks for the reply RE,
Actually, I have never read anything about the DRV8301 that tells of reading back status register 1. So that answer is no.
Oddly enought this same motor worked well with the 8312 kit, don't know if that means anything. It…