Part Number: DRV8313 Hello, I am working on a three phase PM stepper motor with microstepping for space applications. Notice your DRV8313 BLDC motor drive can be used for three phase PM stepper motor applications. My questions are,
How its PWM is…
Part Number: DRV8313 Hi,
Requirement is when there is low voltage on COMPN then nCOMPO drives Logic AND gate to low, which disables enable of driver.
Reference voltage (through divider circuit) set at COMPP is powered by 3.3V of IC
If driver gets…
Part Number: DRV8313 Hi team,
Do we have a replacement for the DRV8313 that’s higher current rated?
Further do we have a SPICE model for any of the suggested drivers?
Kind regards,
Wouter Kragt
Part Number: DRV8213
Tool/software:
Hello Everyone,
We are utilizing the DRV8213 in one of our designs and have ran into some hurdles with the low power of the device.
Current setup:
VDD = VM = 3V VREF - voltage divider set to 1.2V (1.8Mohm…
Part Number: DRV8313 Other Parts Discussed in Thread: DRV8316 , DRV8323 , MCF8315D , DRV8316C , DRV8376 Tool/software: Hi all,
Firstly - props to you all here for the outstanding contributions you make; the community is a real treasure-trove that is…
Part Number: DRV8313 Hello,
I have the following marking on this component DRV8313PWPR :
DRV8313
16TG5
C82L
Is this the correct marking format? Is it possible to provide info about the meaning of each character?
Thank you!
Part Number: DRV8313 Hi Team,
I am looking to control a BLDC motor using a sine wave controller and need a driver for this application. Now I have come across various things about an H-bridge and a half bridge driver which were not entirely clear to…
Part Number: DRV8313 Other Parts Discussed in Thread: DRV8316 , , DRV10974 , DRV8300 , LAUNCHXL-F280049C Hi Dear,
1-Does the BLDC motor driver chip DRV8313 and DRV8316 require an additional Hall sensor?
2-Do all BLDC Drivers in the following figure…
Part Number: DRV8313
Hello Team,
The overcurrent protection does not work for the case if the outputs OUT1 and OUT2 have a extern short-circuit. (only an additional external measure resistor of 50mOhm is located between the both outputs). Power supply…
Part Number: DRV8313 Hello there
In pspice environment I tried to install it using products with pspice file similar to DRV8313. Do you have a situation to write the DRV8313 Pspice file? I am having some problems with modeling brushless motors and their…