Part Number: DRV8313 Hello Team,
I designed PCB same as the ficture below.
My motor works but stops with nfault problem in a few seconds.
The nfault level drops to low.
Should I fix the schematic?
What issues should I confirm?
Thanks,
Robert.
Part Number: DRV8313 Hi Team.
I'm working on synchronous operation with drv8313, but motor doesn't work.
And I don't know the meaning of synchronous and asynchronous rectification exactly.
Should I supply 3-phase trapezoidal wave to INx while…
Part Number: DRV8313 Hello there
In pspice environment I tried to install it using products with pspice file similar to DRV8313. Do you have a situation to write the DRV8313 Pspice file? I am having some problems with modeling brushless motors and their…
Part Number: DRV8313 Dear Sir,
I tried running the motor with two pieces of hardware available with me. 1. Motor is running with STSPIN233, Current is drawing at 8VDC is 0.25 A. 2. Motor is running with DRV8313, Current is drawing at 12VDC is 1.10 A.
The…
Part Number: DRV8313 Hi,
In the datasheet , features says the current drive capability is 2.5A Peak.
In the Block diagram it's 3.5A.
I am bit confused could you please confirm the Current drive capability of DRV8313.
Thanks,
Arif
Part Number: DRV8313 Dear Sir,
Please review the schematic and suggest the changes. Please find the attached schematic of DRV8313PWP.
Regards Murthy DRV8313PWP.pdf
Part Number: DRV8313 Hi
I have designed a custom board for my motor using the DRV8313 chip, which I have designed as per the datasheet.
Now when I give input to my board that is 12 VOlts, my internal LDO from DRV8313 is working fine i.e. I am observing…
Part Number: DRV8313 Other Parts Discussed in Thread: TMS320F28379D Hi TI team
I am using a DRV8313 custom board for controlling a hall sensor-based BLDC motor. I have successfully implemented speed control, now I want to do position control.
Please suggest…
Part Number: DRV8313 Other Parts Discussed in Thread: INSTASPIN-BLDC , , MSP430G2553 , DRV8316 For DRV8313 EVM board it says that it supports instaspin-BLDC, and has an MSP430G2553 board. So it just needs a driving signal as external output or requires any…
Part Number: MCF8315D Other Parts Discussed in Thread: MCF8316D , , MCF8315C , DRV8313 Tool/software: Hi, we're interested in CPAP market applications. Why has been removed the statement "CPAP Machines" from MCF8315D and MCF8316D in respect…