Part Number: DRV8316 Hi team,
My customer wants to use DRV8316 in humanoid robot joint module and they want to know what is the continue current ability. Peak current is 8A. Do we have themal testing data?
Part Number: DRV8316 Tool/software: Hi! I have a working example I wish to replicate using the DRV8316. In my working example, I use an ST L6234 as the driver for my BLDC motor. I set the 3 EN pins to high, and input 3 sinusoidal waveform into the IN…
Part Number: DRV8316-Q1
Will the algorithm's high-current output cause the pre-driver chip to trigger protection, resulting in no output from TI at the moment of motor startup?
We have verified that the output calculated by the algorithm at the moment…
Part Number: DRV8316-Q1 Tool/software: Hello Expert
When I was configuring register 4, I saw OCP_CBC and there was no introduction about it in the datasheet.
Can you clarify the functionality of this configuration?
I understand that changing the…
Part Number: DRV8316 Tool/software: We would like to remove the TI information from the package of a specific component and use only our customer part number. Is such customization possible?
Please also let us know if there are any additional costs…
Part Number: DRV8316 Tool/software: Hello , DRV8316 datasheet states that SOA,SOB,SOC pin integrate current sense amplifier .What is the output impedance and output current of the SOX pin? ADC input range is 1V,and Is it possible to add external voltage…
Part Number: DRV8316 Tool/software: Hi all,
we are planning to use the DRV8316 to drive a PMSM with a PWM frequency of 100kHz at 24V using the 3x PWM mode. Currently we are still using the DRV8316REVM evaluation board.
The problem is, that there…
Part Number: DRV8316-Q1 Other Parts Discussed in Thread: DRV8316 , DRV8343-Q1
Tool/software:
Hi,
In our current project, we are considering the DRV8316-Q1 as a potential driver for three independent half-bridges due to its suitability in terms of…