Part Number: DRV8316 Hi
The DRV8316T is shown in the datasheet as a "Device available for preview only. ". Can I get a sample? May I know the official release date?
Thanks
Hi Roy,
Thank you for your patience.
I have been looking into possible causes to your issue and believe that it may be helpful to re-run through the GUI and EVM setup using the version provided in this E2E FAQ which should also provide assistance in that…
Part Number: DRV8316
We would like to use the DRV8316CTRGFR but there appears to be no stock. Is this a valid part?
Also is there a version of the DRV8316xEVM with the hardware interface variant (DRV8316T)? If so how would I order one.
Hi Annie,
Please let me know if this issue was solved by resolving this thread. We believe there may have been some issue with the communication between the MCU and the driver but can only figure this out if the above waveforms are sent. I am marking…
Hi Alicia,
Alicia Rosenberger said: I will need to review this information with my team.
Expect your response.
Would it be possible the "Vref" in Iout = (SOX-Vref/2)/GAIN have a change? If so, the voltage acquisition may not be good due to a change in the…
Part Number: DRV8316-Q1 hi Team,
now customer is not use SPI link to MCU, they use EVM test, when pull up nsleep to high, it will occur a low pulse in the SDO, you can see the next picture is test result.
could you help explain the reason, and any other…
Part Number: DRV8316-Q1 Other Parts Discussed in Thread: DRV8316
Hi Expert,
Thanks a lot for your warm help!
My customer is tend to select BLDC motor driver in their project.
I am not familair with the application. Would you mind giving me some advice…
Part Number: DRV8316 Other Parts Discussed in Thread: DRV8311 , I would like to inquire about the PWM frequency support of the DRV8316 driver, specifically why the BLDC Integrated MOSFET Thermal Calculator lists the maximum supported frequency as 75kHz…
Part Number: DRV8316 Other Parts Discussed in Thread: MOTORWARE , Hi Team, Working on Field oriented control of a BLDC Motor I had bought this LaunchXL F280049C Microcontroller and the DRV8316R Motor driver, I tried to find support for a similar rig online…