Part Number: DRV8316C-Q1 Other Parts Discussed in Thread: DRV8316REVM , Hi team, I have DRV8316REVM board and DRV8316CR-Q1 IC. The DRV8316REVM board works fine, but when I remove the DRV8316RRGFR connected to the DRV8316REVM board and replace it with the…
Part Number: DRV8316C-Q1 Other Parts Discussed in Thread: DRV8316C , DRV8316 For my project i am looking fo a simple 3-PWM bldc motor controller, during my reacearce drv8316c did look like one of the best options.
The problem I have with this schematic…
Part Number: DRV8316C-Q1 Other Parts Discussed in Thread: DRV8316 , Hi Team,
After DRV8316CT-Q1 is powered on, AVDD can output 3.3V normally, but the configuration pins GAIN/MODE/OCP/SLEW are not pulled up. If the pull-down resistor is not attached, it will…
Part Number: DRV8316C-Q1 Other Parts Discussed in Thread: DRV8316 I am implementing C driver for the DRV8316C but I am facing issue with the SPI write.
By performing a read of all the registers, I get the following values :
IC Status : 0x00
Status register…
Part Number: DRV8316C Hello,
currently we are exploring the DRV8316C and its ASR/AAR features. We are using 6xPWM Mode, not using the internal cycle-by-cycle current limitation. CSA_GAIN is 0x0, ILIM_RECIR is 0x0.
To verify the correct working of the feature…
Part Number: DRV8316C Hi Team,
The following figure shows the data waveform of writing Control Register 6, and then reading Control Register 6, it can be seen that there is no data output from SDO. Customer wants to know why?
Customer refers to the schematic…
Part Number: DRV8316C Hello team,
In the use case that the power supply rails are separated between VM and VIN(for Logic), is there any problem if VIN is supplied when the VM=0V? I'm expected there is no issue such as a large current leakage path. …