Part Number: DRV8320
Hi TI support team,
We are using a DRV8320 in 3PWM mode to control our brushless motor. We use the INLx pins to disable all the PWM outputs in a single row (DRV_INL net on schematic). We are observing a big negative current…
Part Number: BOOSTXL-DRV8320S Other Parts Discussed in Thread: C2000WARE-MOTORCONTROL-SDK , MSP-EXP430F5529LP , DRV832X , MSP430F5529 , DRV8320 , TIDA-01585 , MSP430FR2311 , BOOSTXL-DRV8320RS , MOTORWARE Good morning to everybody
I have a BOOSTXL-DRV8320S…
Part Number: DRV8320 Other Parts Discussed in Thread: DRV832X , Hello,
We are using sensorless motor in our project. we want to use sensorless and 1xPWM Mode. Can we change motor direction with INHC pin?
Thank You
Murat
8.3.1.1.3 1x PWM Mode …
Part Number: DRV8320 Other Parts Discussed in Thread: STRIKE , DRV832X Customer is using DRV8320 HW version.
In the d/s there is a Fault diagnostic table for SPI as below. is it also applied to HW version? if not, is there a similar table to address…
Part Number: DRV8320 I would like to ask you to tell us if the OCP_MODE register settings match the following recognition.
1) OCP_MODE register settings are shared by SEN_OCP and VDS_OCP.
2) Only enable / disable of SEN_OCP can be set independently with…
Part Number: DRV8320 Hi Adam,
I refer to my previous posts regarding DRV8320. I did a lot of tests with the driver (measure of Gate Source voltage at HS and LS, improve signal routing at the board, add addtional GS capacitor to improve dv/dt capability…
Part Number: DRV8320 Hello,
We are developing a new low power motor controller and would be thankful on clarification with determining IDRIVEP, IDRIVEN, TDRIVE, and DEAD_TIME.
The below image provided is our FET specifications and our PWM frequency…
Part Number: DRV8320 What is the priority of fault conditions?
If a fault occurs due to GDF and then the voltage drops to UVLO, which fault has priority and which information is notified to the microcomputer?
Will both be notified?
Part Number: DRV8320 Hello team,
My customer would like to measure the actual gate drive current of DRV8320.
Are there any good method/advice to measure it?
Thanks.
Regards,
Hirata