Part Number: DRV8332-HT Tool/software: Hello.
I need to know the RDS(on) value of the DRV8332-HT however the Data sheets does not make it clear what it is.
In Features it says that RDS(on) is 80mΩ
In Electrical Characteristics is says that RDS(on…
Part Number: DRV8332-HT Other Parts Discussed in Thread: DRV8316C , DRV8332 , DRV8376 Tool/software: Hello there,
Can you please let me know if you have any in stock for this item DRV8332DKDR or DRV8332DKD
Thank you,
Dhexter
Part Number: DRV8332 Tool/software: Hi Expert,
Good day.
Please refer to the image below.
Could you kindly confirm the acceptable level or tolerance for mold flash on the heat sink surface?
Also, please confirm whether the mold flash shown…
Part Number: DRV8332 Hello,
What happens if one phase exceeds the overcurrent limit? Does it just limit the current for that phase? Does it disable that phase and trip a fault signal? What is the recovery process if that happens?
Thanks!
Part Number: DRV8332-HT Other Parts Discussed in Thread: DRV8332 Tool/software: Hi Team,
Due to DRV8332DKDR EOL, BU suggest move to DRV8432DKDR.
Customer feedback DRV8432DKDR cannot direct replace DRV8332DKDR in their design-
1. Not P2P
2. Smaller…
Part Number: DRV8332 Tool/software: For part DRV8332DKDR received, the surface found to have severe scratches, deep marks, and signs of surface discoloration on the metal top of the package.
What is the cause of this observation?
Are these scratches…
Part Number: DRV8332-HT Tool/software: We used the following circuit to drive the propeller, and there was a problem with one of the propellers during use: after the propeller was started, it ran normally. About half an hour later, the propeller had a…
Part Number: DRV8332-HT Other Parts Discussed in Thread: DRV8332 For DRV8332, if using six-step control, its power consumption will be smaller than using FOC control? Is this right? Since for six-step control, only two MOSFETS will be turned on during…
Part Number: DRV8332 Hi, TI support team
To review the DRV8332 product, EVM was checked, but it was confirmed that there was no EVM for the product.
Through another E2E link, it was confirmed that the lower current version has DRV8312-69M-KIT and…
Part Number: DRV8332 Hi, TI support team
The customer is reviewing the parts below.
- part name : DRV8332DKDR
- Application: Parking control system
Noise is occurring as shown in the waveform below.(outA, outB, outC, red box)
Please give…