Part Number: DRV8340-Q1
Hi all,
Given the following waveform, where
Yellow = GLx, 2V/div
Turqoise= GHx, 10V/div
Purple = Phase, 5V/div
Phase current is 5A. When there is no phase current, the negative transient does not occur.
Would…
Part Number: DRV8340-Q1 Other Parts Discussed in Thread: DRV8329-Q1 Tool/software: Hi team,
Do we have more suitable and cheaper devices to replace DRV8340-Q1 with below demand? Thanks.
Motor spec: 120W, output voltage is below 9-16V (TYP 13.5V…
Part Number: DRV8340-Q1 Tool/software: Hello Team,
Could you provide Functional Safety FIT Rate, FMD and Pin FMA document since it was not on the TI.com?
Could you tell me if there are any affect when RSVD pin (35 pin) shorts to adjacent pin?…
Part Number: DRV8340-Q1 Tool/software: hi expert
i saw the following details in our datasheet.
why is Isource current bigger than Isink? is there any special aim?
thanks
Part Number: DRV8340-Q1 Other Parts Discussed in Thread: DRV8353 Tool/software: In DRV8340-Q1 datasheet, for Enable pin, input logic high current (I_lH) is mentioned as 80uA (at 5V input) and pull-down resistance of 60kohms (internal pull-down).
If…
Part Number: DRV8340-Q1 Other Parts Discussed in Thread: DRV8350
Hi team,
Can you please help check the external circuit of DRV8340 customer designed?
1.Is there must be a resistor in series of between VDRAIN?
2.The DRV8350's power supply is the…
Part Number: DRV8340-Q1 Tool/software:
Hi Yara,
We have discussed on my customer schematic of using DRV8340 in aux drive system. But some abnormal occurred:
The schematic looks similar to E2E forum except they have optimized the ground connection…
Part Number: DRV8340-Q1 Hi team,
How much delay time from completing reset pulse input ( consists of a high-to-low-to-high transition on the ENABLE pin ) to operation state? Is it 1msmax? If yes, do you have minmum time spec for that?
Regards, …
Part Number: DRV8340-Q1 Hello,
I was looking to determine the short circuit protection response time for this component and was struggling to find the value in the datasheet. What is this time?