Part Number: DRV8350 Have checked the link of
https://e2e.ti.com/support/motor-drivers-group/motor-drivers/f/motor-drivers-forum/804041/drv8350r-vcp-output-voltage-and-power-consumption-with-different-supply-on-vm
still have some questions.
Ti give…
Part Number: DRV8350 Tool/software: Since different capacitance values lead to different outcomes, it can be inferred that the pin’s performance is unrelated to its sink current capability. Could you please specify the range of capacitance values that…
Part Number: DRV8350 Dear Sir/ Madam,
We received the parts and the MSL shows MSL 1. The date code is 2613. But the website shows MSL 2. Would you please confirm whether it is correct?
Thank you
Yours sincerely,
Part Number: DRV8350 Tool/software: Dears,
The customer uses DRV8350 in the application scenario of electric forklifts, with a 24V system and a three-phase asynchronous motor as the load. The motor power ranges from 1.5KW to 3.0KW. Use DRV8350SRTVR…
Part Number: DRV8350F Other Parts Discussed in Thread: DRV8350 Hello! This is Jin. I am trying to use an half bridge driver for generating an waveform with fast rising/falling edge speed. The voltage will be from -20V to +60V. I was thinking about using…
Part Number: DRV8350 hi team,
my customer is using DRV8350 in 40V servo system.
They found that every time they set the enable signal to high, the VGLS will rise to only 7V and the high voltage between GLx and SLx will only be 3V.
the VGLS signal…
Part Number: DRV8350 Hi Team,
User DRV8350, SPI is not configured, using default values. No motor is connected. When the DRV8350 receives the PWM signal nFault, it reports an error.
Part Number: DRV8350 Tool/software: Im using DRV8350SR.Whorking fine for BLDC MOTOR. Im planing to new design for PMSM MOTOR OR SYNCHRONOUS motor. This driver can Handel to drive please let me know that.
Part Number: DRV8350 Hello team,
I have a quick question about our DRV835x, do DRV835x support negative voltage?
From datasheet it didn't seem to, so I wanted to check with you. To ensure the FET is turned off, instead of 0V customer is using negative…
Part Number: DRV8350 Tool/software: I'm using the DRV8350 and planning to implement a dual-supply architecture. In this setup, should VCP be connected to the VDRAIN voltage or the VM voltage?
For example, if I use a 48V to 12V regulator to generate…