Part Number: DRV8350H-EVM Other Parts Discussed in Thread: MSP430F5529 , DRV8350 , DRV8350S-EVM
Dear TI Team,
I am trying to control a BLDC Motor using DRV8350H-EVM in sensored operation. But as soon as I increase my Motor Speed over 50%, my motor stops…
Part Number: DRV8350H-EVM Hey,
I have DRV8350H-EVM evaluation kit which I am using for testing purposes and we are able to run the motor we have at 100% speed in sensored mode using the GUI provided by TI. I want to know what specific commands/data it…
Part Number: DRV8350H-EVM Other Parts Discussed in Thread: DRV8353 , DRV8350 Hello,
I am trying to evaluate the sensored operation of the DRV835x driver using the DRV8350H-EVM . I followed the steps mentioned in the EVM user guide (SLVUB78A) and https:…
Part Number: DRV8350H-EVM
Hello,
I'm interested to know if there are any issues with using the DRV8350HRTVT as a half-bridge or even a full h-bridge driver. I'm guessing if the driver is being used as 3 x individual half-bridge drivers the maximum…
julien leconte said: We set the current in the graphical interface or in the software by forcing the value of 2606.
This confirms my suspicion that the GUI has an error of using 'A' -- current in Ampere -- as the unit for this parameter, which is really…
Part Number: DRV8350H-EVM We are trying to control a small medical 3-Phase BLDC motor to get a wide range of RPMs. For the testing, we are using the DRV8350H EVM.
We have adjusted firmware to use 6-PWM mode. Our current firmware is using the Hall Sensors…
Part Number: DRV8350H-EVM hi, i am using this driver ic for 100% duty cycle pwm signals input.i have connected INL signals to ground and connected INH signals to GPIO pin of controller. i am trying to make on/off INH signals but i could not see same on…
Part Number: DRV8350H-EVM Hi,
I have two different motor driver. One is DRV8320S and the other is DRV8350H. While I could control the engine very well with the DRV8320S, I couldn't do it with the DRV8350H. I also make the necessary resistance settings…
Part Number: DRV8350H-EVM Own DRV8350H hardware can not work
Hello, everyone.
I’ve built my own hardware for a three-phase-inverter with DRV8350H. The schematic is shown.
When I test this circuit, the DRV8350H didn't work.
The supply voltage…
Part Number: DRV8350H-EVM Other Parts Discussed in Thread: DRV8350 , MOTORWARE Hello!
I am trying to drive a Maxon Brushless DC Motor with the DRV8350H-EVM and the DRV8350X-EVM GUI. I have been trying to run the motor with 1x-PWM mode (I removed R66 to…