Part Number: DRV8350H-EVM Other Parts Discussed in Thread: DRV8350 , I believe I have everything set up to properly spin a sensored motor using the EVM board but, I keep getting MCU faults and I do not see why.
I have the Dev board hardware reworked with…
Part Number: DRV8350H-EVM Other Parts Discussed in Thread: DRV8350 , MSP430F5529 Hi,
I just got this DRV8350H-EVM board, connected it to a motor with hall-sensors and managed to control it via the provided GUI
Now that I see it works - I want to control…
Part Number: DRV8350H-EVM Other Parts Discussed in Thread: DRV8353R , DRV8350 Tool/software: Code Composer Studio Hi,
Single shunt board: https://www.ti.com/tool/DRV8350H-EVM
Can you please tell me if there is any FOC code which I can run on this evaluation…
Scalery,
The board you are showing is not the DRV8350H-EVM, it is some other board. Do you have the schematic of this board?
Likely the MSP430 needs to be programmed.
Regards,
-Adam
Part Number: DRV8350H-EVM Other Parts Discussed in Thread: MSP430F5529 , LP-MSP430FR2476 , DRV8350 , I have developed a new board used to driver BLDC, It mainly used DRV 8350 and MSP430F5529, but I don't use the onboard emulator but use the EZ_FET emulator…
Part Number: DRV8350H-EVM Other Parts Discussed in Thread: MSP430F5529 Tool/software: Code Composer Studio hello ,
I have tested the DRV8350H-EVM , and it's good .
My question is about the firmware -- "DRV835X_MSP430F5529_Trapezoidal_Sensored_BLDC…
Part Number: DRV8350H-EVM Other Parts Discussed in Thread: DRV8353RH-EVM , DRV8301-69M-KIT , DRV8350 , DRV8353 Tool/software: Code Composer Studio hi,
I have tow questions please,
1/ what is the best evaluation model for the sensorless FOC controller of…
Part Number: DRV8350H-EVM Other Parts Discussed in Thread: DRV8350 , MSP430F5529 I installed the GUI software per the instructions in DRV8350x-EVM GUI User’s Guide. When the software connects to the EVM, the Sensored option disappears and I can only…
Part Number: DRV8350H-EVM Hello everyone, I'm using DRV8350H-EVM to drive Brushless DC Motor of an E-BIKE, I implement my own source code without using the firmware, the motor is spinning perfectly without any kind of noise.
Noting that the motor is…
Part Number: DRV8350H-EVM Dear all,
I needed a "quick fix" to running a sensored three phase motor, so I bought the DRV8350H-EVM, as it is listed with all the right qualifications and comes with ready to be built firmware.
However, the code…