Part Number: DRV8353RS-EVM
Hello,
I am trying to control a 3 phase bldc motor using the drv8353-evm with in 6x mode. I am using an input voltage of 24V, I can see an output voltage of 34V on the charge pump pin. however, all of the GHx pins are only…
Part Number: DRV8353RS-EVM Dear TI team ,
I am facing the following issues while DMC level -1 , I have try possible solutions but yet not shorted out
please me to solve it. as I debug the I faced these two fault as well as the default offset parameter…
Hi Arjun,
I see your question was answered on another E2E thread so I will be closing this one. Please feel free to submit a new E2E post if you have any other questions.
Thank you,
Yara
Hi Arjun,
I believe the given motor should be able to be driven by a DRV835x system. Can you provide more details about the IC failure cases and what part of motor operation this occured?
Could you also provide the info of the smaller motor that successfully…
Part Number: DRV8353RS-EVM Hello sir,
I would like to ask , I have the following (DRV board + Launchpad) which is mentioned above as well.
Can you please recommend the suitable motor for the same, even I have 1000W hub motor and trying to spin it as per…
Part Number: DRV8353RS-EVM Other Parts Discussed in Thread: LAUNCHXL-F280025C , DRV8353 Hi,
My setup is Launchxl-F280025C + DRV8353RS-evm, used for BLDC motor control.
Since DRV8353RS-EVM has 3.3V regulator, Should I keep JP1,JP2, JP3 of Launchxl-F280025C…
Part Number: LAUNCHXL-F280025C
Hello Sir,
we are using universal motorcontrol lab sdk to spin our bldc motor , now we are trying to disable the SPI communication in order to control DRV8353RS manually or by some hardware change, But I couldn't find any…
Part Number: DRV8353RS-EVM
Dear sir,
i have hub motor and Launchpad-F280025c
DMC-2
Added, as I set the v/f parameter and reduce and increase the dacCMPValL and dacCMPValH value , we are not getting overcurrent fault ,under the default max_current setting…
Part Number: DRV8353RS-EVM Other Parts Discussed in Thread: DRV8353 , Hey,
We are working on DRV8353 and TI launchpad F2800157 for BLDC motor application. I configured with Universal Motor Controller code (I followed the universal motor control SDK document…