Part Number: DRV8353RH-EVM Hello,
I recently purchased the DRV8353RH-EVM board and have been testing it in 1x PWM mode. I made the modifications to the configuration resistors, including removing R23, R26 and R31 to configure the driver to be in 1x…
Part Number: DRV8353RH-EVM Hello E2E Experts,
I am using only the DRV8353RH gate driver IC and am not getting an amplified PWM output when applying a 3.3 V PWM input signal.
The hardware connections are as follows:
VM = 22 V, with 10 µF and…
Part Number: DRV8353RH-EVM Hello E2E Experts,
other gate outputs operate normally.
To isolate the problem, I configured MCU GPIO0–GPIO5 as general-purpose outputs (not PWM) and directly drove the DRV8353RH input pins (INHx and INLx). I tested the…
Part Number: DRV8353RH-EVM Dear TI Applications Support Team,
I am writing to seek technical advice regarding a 48V motor drive design using the DRV8353RHRG gate driver.
During bench evaluation under a no-load condition (motor disconnected and MOSFETs…
Part Number: DRV8353RH-EVM Other Parts Discussed in Thread: DRV8353 I am developing a custom 3-phase BLDC servo driver using the DRV8353RH. We are experiencing recurring hardware failures specifically related to the charge pump (VCP ~1V, nFAULT triggers…
Part Number: DRV8353RH-EVM Tool/software: Hi, I started working with EV board, but the engine is not running, fault LED is on, Rs 1.17975881e+38 Ohm. The motor and everything else is fine. How can I solve this? Thanks for your answer
Part Number: DRV8353RH-EVM Other Parts Discussed in Thread: LAUNCHXL-F28027F , Hello! I'm aiming to transmit a PWM signal from a different microcontroller (STM32) than the one on the LAUNCHXL-F28027F board. Initially, I attempted to connect the STM32…
Part Number: DRV8353RH-EVM Other Parts Discussed in Thread: DRV8353 Tool/software: I’ve designed a piggyback board (segment shown) that drops onto the DRV8353RH-EVM to test my DRV8353 control firmware. I’m using the DRV on the EVM for this test setup…
Part Number: DRV8353RH-EVM DRV8353H: Incorrect behaviour of GHx signals in 1x PWM mode
we are using DRV8353RH -- 40pin Driver and configure 1x PWM mode without Gate (open) Resistor we are getting
GHx PWM Pulse Ramp down
The issue is slow GHx…
Part Number: DRV8353RH-EVM Other Parts Discussed in Thread: MOTORWARE Tool/software: How to configure and compile the Proj_Lab05a.c file in CSS in our Evalution board instead of proj_lab05b.c