Part Number: DRV8353RH-EVM Other Parts Discussed in Thread: DRV8353 , MOTORWARE , MSP430F5529 Hi,
Good Day. I have a customer who is working with DRV8353RH-EVM. Please see below his query for your reference. Thank you very much.
We are using DRV8353RH-EVM…
Part Number: DRV8353RH-EVM Other Parts Discussed in Thread: DRV8353 Hello,
I configured DRV8353RH-EVM to work in 1 PWM mode. Power supply 48V/10A. motor with hall sensors.
The setup did work correct for about 20 hours. After that time I got error message…
Part Number: DRV8353RH-EVM Other Parts Discussed in Thread: TMS320F28027 , DRV8353RS-EVM Hello,
I try to evaluate the DRV8353RH-EVM Board.
I installed the DRV8353Rx 1.0.1 application on Windows 10.
When I try to connect to the DRV8353RH-EVM, I have the…
Part Number: TMS320F28027F Other Parts Discussed in Thread: MOTORWARE , DRV8353RS-EVM We are facing issue in running motor with DRV8353RH EVM GUI. While start running the motor, motor start running icon goes into not selectable mode, resulting in unable…
Part Number: DRV8353RH-EVM Other Parts Discussed in Thread: INA210 , DRV832X
We are trying to identify the right way to work with the transient effects of the source pin on the 8353. On the 8353, the FET source pin from the gate drive is shared with the…
Part Number: DRV8353RH-EVM
I bought this development board (DRV8353RH-EVM), attached the ISO board on it, and immediately the red light of the FAULT on the EVM lights up when I wired a 36V DC power supply. There is no motor connected nor USB connected…
Part Number: DRV8353RH-EVM Hello,
I have two DRV8353RH-EVM boards and am encountering same problem in both. I am using the default settings, I have not touched anything in the board.
I am generating good INHX and INLX with Simulink for the 3x PWM mode…
Part Number: DRV8353RH-EVM Hello Team,
My customer is curious to know, if they can use the DRV8353RH-EVM board for 500W output power with 48V input.
Do we have some kind of test report for this board with operation upto 15A continuous output current? …
Part Number: DRV8353RH-EVM Other Parts Discussed in Thread: DRV8353 , DRV8353RS-EVM , MOTORWARE Hello Guys,
Good day.
User guide stated that the DRV8353Rx-EVMs are designed to be evaluated only with the ISO- F28027F MCU PCB accompanying the kit.The question…