Part Number: DRV8353RS-EVM Hi,
We ordered DRV8353RS eval kit for our 48V motor control application.
Rated and peak power for our motor is 4kW and 7kW However we want to test our motor in no load condition using eval kit hardware.
Is there any guide…
Part Number: DRV8353RS-EVM Other Parts Discussed in Thread: MOTORWARE , , LAUNCHXL-F280025C , DRV8353 We installed the CCS, the motorware and blackhawk control software and tried to connect and run our motor controller but it did not work. We used the…
Part Number: DRV8353RS-EVM Other Parts Discussed in Thread: DRV8301 We are using the DRV8353RS EVM and the board is not working properly. We have trouble with the gate not switching properly. The gate driving output of the board is at too low of a voltage…
Part Number: DRV8353RS-EVM I am a beginner and I have been trying to build a robot where my Nucleo H755zi-q will act as the motor controller. After research on chatgpt I got my hands on the DRV8353rs-evm to power a 3 phase 120 Degree Hall sensor based…
Part Number: TMS320F28P551SG Other Parts Discussed in Thread: LAUNCHXL-F28P55X , DRV8353RS-EVM , , BOOSTXL-DRV8323RH , LAUNCHXL-F280039C I want to use an eval board (like LAUNCHXL-F28P55X) for an upcoming TMS320F28P551SG project. I would like to use the…
Part Number: DRV8353RS-EVM Tool/software: HI all
I am trying to understand how can I achieve forward and reversed direction of motor using this truth table as in refer. manual INHC will decide the motor direction which can be 0 or 1.
I have shared…
Part Number: DRV8353RS-EVM
Dear TI Support,
I am using the DRV8353RS in 3x PWM mode for sensored 6‑step BLDC control and I have two clarification questions about the INHx / INLx inputs:
In 3x PWM mode, should the INLx pins (INLA, INLB, INLC…
Part Number: DRV8353RS-EVM Other Parts Discussed in Thread: DRV8353
Tool/software:
Hi,
We are facing similar issue where the motor gets identified but not spinning, We tried two different motors, Both did not work.
The attached screenshot is of…
Part Number: DRV8353RS-EVM Hi
I am currently creating motor controlller over STM32f407 and DRV8353RS ,the DRV8353rs evm board is currently being controlled via ISO28027F daughter board. Can anyone help me to understand if it is feasiblity and possible…
Part Number: DRV8353RS-EVM Hi
I am using the DRV8353RS with an STM32F407VGTX in 1xPWM synchronous mode . The MCU drives INHA (PWM), INLA, INHB, INLB, INHC and INLC, and I am trying to verify the gate‑drive outputs on the DRV8353RS‑EVM using an LA1010…