Part Number: DRV8353RS-EVM Hello sir,
I would like to ask , I have the following (DRV board + Launchpad) which is mentioned above as well.
Can you please recommend the suitable motor for the same, even I have 1000W hub motor and trying to spin it as per…
Part Number: DRV8353RS-EVM Other Parts Discussed in Thread: DRV8353 , Hey,
We are working on DRV8353 and TI launchpad F2800157 for BLDC motor application. I configured with Universal Motor Controller code (I followed the universal motor control SDK document…
Part Number: DRV8353RS-EVM Other Parts Discussed in Thread: DRV8353 , DRV8353R
Dear TI team,
I literately want to know what is the main cause of voltage offset fault . I have changed two boards for the same and still not get the cause and solution of this…
Part Number: DRV8353RS-EVM Hello,
When I write to the gate driver register using SPI from another MCU, the gate driver register is successfully written. But when I exit the debugging mode of the firmware or power the board off, then restart and read the…
Part Number: DRV8353RS-EVM Other Parts Discussed in Thread: DRV8353 Hello Team,
We are working on DRV8353 and F28027F for BLDC motor application. I connected the 24v BLDC motor is working fine.
When we are connecting the 48v PMSM motor slightly vibration…
Part Number: DRV8353RS-EVM
Dear sir,
i have hub motor and Launchpad-F280025c
DMC-2
Added, as I set the v/f parameter and reduce and increase the dacCMPValL and dacCMPValH value , we are not getting overcurrent fault ,under the default max_current setting…
Part Number: LAUNCHXL-F2800157 Other Parts Discussed in Thread: DRV8353RS-EVM , DRV8353
Hello All,
I am utilizing LAUNCHXL-F2800025C and a DRV8353RS-EVM to work through the Universal Motor Control Lab.
I refer the F280025c code and I configure the F2800157…
Part Number: DRV8353RS-EVM Hi Team,
The customer samples the resistor current of the DRV8353RS-EVM using the Bidirectional current-sense Configuration with a gain design of 40 V/V.
But the amplified signal is found to be inverted. Is there a way to correct…
Part Number: DRV8353R Hi,
I plan to use a DRV8353R in my motor drive design.
What is the meaning of NT1....NT7 on the schematics of the DRV8353RS-EVM please?
Best regards,
David
Part Number: DRV8353RS-EVM
Dear sir,
I have DRV8353RS-EVM , LAUNCHPAD-F280025C and Hub motor .
(Note:- I am using 24 to 30 volt power supply and my hub motor max voltage are 48 volts and 102 hz frequency)
Recently I have complete the DMC_Level_1 as per…