Part Number: DRV8353RS-EVM
Dear sir,
I have DRV8353RS-EVM , LAUNCHPAD-F280025C and Hub motor .
(Note:- I am using 24 to 30 volt power supply and my hub motor max voltage are 48 volts and 102 hz frequency)
Recently I have complete the DMC_Level_1 as per…
Part Number: DRV8353RS-EVM Hi,
I am working on DRV8353RS-EVM (F28027) development kit. I am unable to program this kit by motor wave software. Kindly connect your engineer with us.
Thanks & Regards
Shadab saifi
Contact no:- 8700440769
Part Number: DRV8353RS-EVM HI Team,
The customer would like to know if there is an example for DRV8353RS to drive BLDC in 1×PWM mode for reference. Thanks.
Best Regards,
Cherry
Part Number: LAUNCHXL-F280025C Other Parts Discussed in Thread: DRV8353RS-EVM , Hi,
Setup is LAUNCHXL-F280025C + DRV8353RS-EVM , running Universal Motor Control Lab.
DMC_LEVEL_1 is set..
Offset_V_sf is 1.0 vs 0.5 expected. Current offset is OK. What cou…
Part Number: LAUNCHXL-F2800137 Other Parts Discussed in Thread: DRV8353RS-EVM Dear all,
I'm doing some test using LAUNCHXL-F2800137 and DRV8353RS-EVM.
Universal_motorcontrol_lab is used, SDK 5.
The set up of the control board was copy on LAUNCHXL-F280025…
Part Number: DRV8353RS-EVM Other Parts Discussed in Thread: MOTORWARE , , DRV8353 Hi,
I'm working with Motorware projects using the F28027F and a DRV8353RS-EVM.
As a first step, I used the DRV8353Rx 1.0.1 GUI for identifying and running my motor and…
Part Number: DRV8353RS-EVM Customer would like to know w hy is a 0Ω capacitor added to the SPI signal line in the schematic? What does the resistor do? Is it possible to remove it?
In additional, w hat are NT1, NT2, and NT3? What are the roles?
Thanks…
Part Number: DRV8353RS-EVM Dear e2e team,
I would like to evaluate the performance of the Vds current sense mode ( page ) with the DRV8353RS-EVM - Can I suppress C22,C23,C25,NT5,NT6,NT7 and short cut R14,R15,R16 in order to test it?
Thanks,
Giorgia
Part Number: DRV8353RS-EVM Other Parts Discussed in Thread: DRV8353 Hi Team,
I am trying to identify the motor parameters using DRV8353 GUI.
My motor is a 48V 5.5kW PMSM and currently i am giving it a supply voltage of 32V.
The GUI during the identification…
Hi VJ.Pandi,
veerapandiyan v said: when the INHx and INLx both are in 0 states the GHx and GLx that also in 0 states only. SHx is HiZ state. why is this datasheet saying that?
The reason that the datasheet specifies this is because GHx is referenced with…