Part Number: DRV8363 I have designed in the DRV8363 motor driver. With the EVM GUI, I can only start the 600W BLDC under no load conditions, and programming register 1A with 0x0CCC needing to be written first. However, when I try to read this back I only…
Part Number: DRV8363-Q1EVM Other Parts Discussed in Thread: LAUNCHXL-F280049C , DRV8363-Q1 , DRV8363 , DRV8353 Dear TI experts,
My customer bought DRV8363-Q1EVM and LAUNCHXL-F280049C for evaluation of DRV8363-Q1.
And my customer need sensorless, FOC…
Part Number: DRV8363-Q1EVM Other Parts Discussed in Thread: DRV8363 Dear TI support team, I'm having issues with a VDS Fault on the DRV-8363-Q1EVM . When operating a bldc driven pump at a constant constant speed with constant load, I'm seeing a strong…
Part Number: DRV8363-Q1EVM Other Parts Discussed in Thread: MSPM0G3519 , DRV8363 , Hi,
MCU: MSPM0G3519
DRV: 8363S
Vmotor = 12V DC
fPWM = 20Khz
Duty cycle = 80%
I am working on motor control application with DRV8363 driver, at present I am…
Part Number: DRV8363-Q1 Other Parts Discussed in Thread: DRV8363 Hi team,
My customer is using DRV8363 in design, they want to optimize the settling time to achieve better single-shunt based FOC control in limited time window. We have two questions…
Part Number: DRV8363-Q1EVM Other Parts Discussed in Thread: DRV8363 Hi team,
We are using a DR8363S for BLDC control, currently we are modifying the same Hardware to drive a BDC(brushed DC) motor .
Is it possible to operate only two legs inorder…
Part Number: DRV8363-Q1 Dear TI experts,
My customer made their schematic with DRV8363-Q1. Could you review it?
DRV8363-Q1_Cooling FAN.pdf
Best regards,
Chase
Part Number: DRV8363-Q1 Other Parts Discussed in Thread: DRV8363DRV8363-Q1 -- I am using this gate driver and it has sensing amplifier, i want to sense 2 phase current and 1 dc current. Can this gate driver can measure?
Part Number: DRV8363 Hello,
We are implementing a DRV8363-based motor driver and have a few questions:
How does the current sense auto-zero function? I assume some form of chopper stabilization?
What kind of extra noise/ripple/offset does it…
Part Number: DRV8363-Q1EVM Other Parts Discussed in Thread: MSPM0G3519 , , LAUNCHXL-F280049C , DRV8363-Q1 , DRV8363 Hi,
I am working on a BLDC motor control application using the MSPM0G3519 MCU and have procured the DRV8363-Q1EVM for gate-driver evaluation…