Part Number: DRV8412 Other Parts Discussed in Thread: DRV8962 , DRV8262 Tool/software: Hello,
I would like to ask if it makes sense to replace ( one DRV8432DKD + mounted heatsink) with ( two in parallel DRV8142DKD heat dissipation over power pad).
The…
Part Number: DRV8412
Tool/software:
Hello,
Can i know the reason of this change ? : Changes from Revision G (July 2014) to Revision H (July 2024): Deleted values in 39 to 200 in Table 6-2 .
It's about the Programming-Resistor Values and OC Threshold…
Part Number: DRV8412 Tool/software: Hello, I'm using the DRV8412 in parallel mode to drive a thermoelectric unit. It's mostly working but has some issues. It needs to power a TEC module at 5A. I'm testing with a 24V power supply and electronic load.…
Part Number: DRV8412 Tool/software: Hi, At the moment I noticed a "obsolete" status by; " DRV8412DDW ". The link: DRV8412 | Buy TI Parts | TI.com But when I search with the type number "DRV8412" i found the following page with the status…
Part Number: DRV8412 Tool/software: I'd like to be able to change the logic levels of M1 and M2 using a microcontroller. My first idea is just to connect the M1 and M2 pins to digital outputs on the microcontroller. However, it seems like doing so would…
Part Number: DRV8412 Tool/software: I downloaded a video with audio from Pinterest using Pinsaver.io , and now I want to edit it with your program. What can I do to remove the sound in the background?
Part Number: DRV8962 Other Parts Discussed in Thread: DRV8412 , Tool/software: Hello,
is there any information or assumptions regarding the difference in power dissipation between the DRV8412 and the DRV8962. The Rdson of the internal MOSFETs of the DRV8962…
Part Number: DRV8412
Tool/software:
This is a schematic of DRV8412 drive a therm heater.
I encountered the following problem:
1.DRV8412 is damaged, OUT_A&OUT_B has output, OUT_C&OUT_D has no output, strangely, the Fault pin and OTW pin are high. Is…
Part Number: DRV8412 Tool/software: As we all know , t he heat dissipation area of the DRV8412 chip is at the bottom of the chip, but in practical applications, if i want to strengthen the heat dissipation of the area where the chip is located, should the…
Part Number: DRV8412 Other Parts Discussed in Thread: DRV8962 Tool/software: hi,
As shown in the figure below, DRV8412 is used as an LED lighting driver. Is DRV8412 equivalent to a BUCK circuit? How does DRV8412 work as an LED lighting driver?
Thanks…