Part Number: DRV8412 HI We have some parts DRV8412 and we are trying to indentoify what the other marking on the first line is.
The marking are 34A28JTG4 or 89C3SLTG4.
We are need trying to figure out the marking.. I could not find any reference…
Part Number: DRV8412 Dear Sir/Madam,
Please advise whether it is recommended/advisable to use DRV8412 to drive 2 TECs simultaneously (up to 3A each), in mode 4 (dual full bridge mode, one PWM input for each full bridge with complementary PWM on second…
Part Number: DRV8412 Tool/software: Hi,
In this thread, Rick is suggesting that not having individual control over each half bridge reset could cause a problem driving a BLDC motor with the DRV8412. Can TI please elaborate on the problem that this could…
Part Number: DRV8412 Other Parts Discussed in Thread: DRV8320 , CSD88584Q5DC , Hi,
We are using the DRV8432 driver for years to control two L-C tank resonators, one for each Full Bridge. As known DRV8432 is obsolete and we are looking for an alternative…
Part Number: DRV8412 Dear TI experts,
My customer now tests their own PCB with DRV8412. Could you review the schematic below?
The problem is, they use this circuit to operate peltier.
if the duty of PWM is under 50%, it is okay. (about under 5A…
Part Number: DRV8412 Other Parts Discussed in Thread: DRV8962 , DRV8262 , DRV8962EVM , Hello,
We are planning to purchase 10 qty of DRV8432EVM.
1. How to connect the solenoid to Eval board? Where we need to connect it?
2. Could you please provide…
Part Number: DRV8412 According to DRV8412 datasheet (p13), "In OC latching shut down mode, the CBC current limit and error recovery circuits are disabled and an overcurrent condition will cause the device to shutdown immediately. After shutdown, RESET_AB…
Part Number: DRV8412 Hello,
In the datasheet it says "In CBC current limiting mode, the detector outputs are monitored by two protection systems. The first protection system controls the power stage in order to prevent the output current from further…
Part Number: DRV8412 Other Parts Discussed in Thread: DRV8876 Hello -
We are using the DRV8412 in our EndoVascular Robot and seeing some overshoot in the PWM output voltage that we are trying to understand and control. I've been trying to develop a…