Part Number: DRV8426 Hi team,
I have questions about tri-level and quad-level input pins. Could you suppot please?
If the input PIN is set to Hi-Z, will there be any impact if unpopulated pull-up/pull-down resistors are connected to the PIN?
Can…
Part Number: DRV8426 Tool/software: Hi,
Does keeping enable & nSLEEP pin in high condition with external pullup, keep the DRV8426 in auto retry mode for below condition
1. VM Undervoltage Lockout
2. VCP Undervoltage Lockout
3. Overcurrent Protection…
Part Number: DRV8426 Tool/software: Hi,
Please find the below schematic for DRV8426
sometimes, during power recycle it gets trapped in improper condition,
where we can observe toggling in "fault" pin & similar activity can be observed on winding…
Part Number: DRV8426 Hello team
I have a question.
Is there a risk of nFault output due to the thermal pad not being connected to ground? My customer made a mistake in pattern design and tested with the thermal pad not connected to GND, and nFault…
Part Number: DRV8426
Hi support team.
Is my understanding correct as following Figure?
If yes, the measured body diode VF value during the dead time period is 1.06V, and it is incomprehensible why it exceeds 1V.
Also, since this exceeds the absolute…
Part Number: DRV8426 Hi support team.
My customer has a critical issue.
-1.75V (186ns) undershoot is occurring at AOUT output. The waveform is below.
The absolute maximum rating is -3V for 100ns, is this acceptable? If NO, could you please give…
Part Number: DRV8426 Other Parts Discussed in Thread: DRV8425 , , DRV8424 Hi team,
My customer wants to know the value of internal pull down resistors on DIR, M0, M1, STEP, nSLEEP of DRV8424, DRV8425 and DRV8426. Could you help with it?
Thanks!
Part Number: DRV8426 Dear team,
My customer is evaluating to use the DRV8426 stepper motor driver for new application.
Looking at the datasheet (PLs see picture below) , DRV8426 is not mentioned in the Automatic Retry paragraph but from Table 7-9…
Part Number: DRV8426 Hi Team,
Can you please check and advise following request?
"
In our circuit, voltage values on all pins seem normal. But when I give 1 (logic high) to the nsleep pin, the nfault pin drops to 2.2V. (Logic 1=5v) When I give 0…
Part Number: DRV8426 Hi Expert,
Could you please let me know the consern for system usecase in case of using Non-circular 1/2step?
The torqe will be 1.41 (√2)at 45 °, 135 °, 225 ° and 315 ° against 0°, 90 °, 180 ° and 270 °.
Generally, do you…