Part Number: DRV8432 Other Parts Discussed in Thread: ABS We have an application where it is possible the motor shaft is spun with no control power to the product.
At this time the motor is a generator and is converted to DC Bus power thru the flyback…
Part Number: DRV8432 Hi team,
Here's an issue from the customer may need your help:
Output a pulse signal of less than 1us at PWM frequency, as shown in the following figure:
And the schematic is as follows:
The input and output of the 74HC32 are…
Part Number: DRV8432 Other Parts Discussed in Thread: DRV8412 , , LM5106 , LM5109 , DRV8705-Q1 Hello,
I'm upgrading a hand-made TEC driver and want to get some features/minituarization from purpose-built ICs.
We're looking at 15V-24V and 6-10A. 24V…
Part Number: DRV8432 Other Parts Discussed in Thread: DRV8711 , DRV8434 Hi,
I am using DRV8432DKD.
In datasheet the mode select pin connection is given in section 9.4.4 as " It is not recommended to connect mode pins to board ground if 1-Ω resistor…
Hi Jacob,
Jacob Wyrick said: Is there any reason we wouldn't or shouldn't add an external charge pump circuit and provide its output to BST_x to achieve 100% duty cycle?
This is not recommended. The external circuit may cause problems with the…
Part Number: DRV8432 hi Team,
we are using your DRV8432 for our design, it's for TEC drive, disign is below, now we found the TEC output was lower than PVDD, for example,
PVDD=15V,but the output is 13.2V, 88% efficiency, as mentioned in datasheet,…
Wang5577 said: What is the voltage waveform on R31 (between AGND and PGND)? What is about OUT_A/B and OUT_C/D voltage?
hi Wang,
attached the waveform for your reference, see below.
AGND and GND
OUT_A and TEC+
OUT_A and OUT_C
BR
Jerry
Part Number: DRV8432 Hi team,
Here's a issue from the customer may need your help:
The customer would like to use this chip to control two DC motors for commutation, speed regulation, braking.
One of the previously used chips is a pin inputting pwm…