Part Number: DRV8818 Other Parts Discussed in Thread: DRV8434S , DRV8434A Hi team,
The customer intends to use use the DRV8818 to drive the stepper motor, and now would like to know the maximum continuous output current of the device, and is this continuous…
Part Number: DRV8818 Other Parts Discussed in Thread: DRV8880 , DRV8462 , DRV8434A , DRV8434 , DRV8434S , DRV8452 , DRV8426 Hi,
Problem description:
The client has been using a DRV8818 chip to drive a stepper motor to control the vertical direction…
Part Number: DRV8806 Other Parts Discussed in Thread: DRV8411A , DRV8461 , DRV8452 , DRV8462 , DRV8434A , DRV8434S , DRV8889-Q1 , DRV8711
Need to find a driver for 28BYJ-48 stepper motor, which driver will be most suitable. I need the driver with stall…
Part Number: DRV8846EVM Other Parts Discussed in Thread: DRV8846 , DRV8434A , DRV8434S , DRV8434 Dear all,
I'm starting a new development using the DRV8846EVM. In order to sense the end of the motor movement ( we have a physical stopper), we want to…
Part Number: DRV8899-Q1 Other Parts Discussed in Thread: DRV8436 , , DRV8434S Dear team
1. The customer would like to know, is the main difference between DRV8899-Q1 and DRV8436 SPI interface ?
2. Does DRV8899 need to use SPI for initial?
3…
Hi Murugavel. 1.VREF voltage is set at 0.4V~0.5V.
2. I would like to ask, the Torque count will be stored in DRV8434, how to clear the Torque count stored in driver after I set STL_MODE to Stall threshold mode? Currently I set STL_MODE to Stall threshold…
Part Number: DRV8434SEVM Other Parts Discussed in Thread: DRV8434S , MSP-FET
Hello,
When enabling the Open Load detection through the software (version 0.1.12) (either with the register map EN_OL = 1b or with the switch), it deactivate itself after…
Part Number: DRV8824 Other Parts Discussed in Thread: DRV8434A , DRV8434S Hi Team,
The stepper motor driver chip currently used drives the stepper motor to drive the gear wheel to rotate in four positions, two of which are limited by the blocking point…
Part Number: DRV8825 Other Parts Discussed in Thread: DRV8434 , DRV8426 , Hello TI Team,
We are using DRV8825PWPR in our design, bur we are facing very high peak noise in the motor at the time of the operation. I am sending you a my schematic.
…
Part Number: DRV8434EVM Other Parts Discussed in Thread: DRV8434 , DRV8462 , DRV8462EVM
Customer is asking if there is a spare GPIO on the DRV8434 Eval Board? Looking at the board schematic, I do not see any spare GPIOs from the MCU connected.
Second…