Part Number: DRV8436
I would normally consider the latest revision as gospel, however, in this case the two revisions cited show completely different operation.
In the July 2022 revision, pins 25, 24, 23, 22 describe 4 inputs 2 for each output with the…
Part Number: DRV8436 Other Parts Discussed in Thread: DRV8426 Hi team,
What is the difference between DRV8436 and DRV8426? It looks like only the difference of full-scale current, operating supply voltage range and full scale current.
Best regards,
Shunsuke…
Part Number: DRV8436 Other Parts Discussed in Thread: DRV8434 Hi Team,
Our customer will design a board that could support multiple devices with similar pinouts in case a certain device is out of stock. He would like to confirm if he n eeds to add a zero…
Part Number: DRV8436 Hi, Good day. Our customer would like to know in which direction would the stepper motor would turn if it a signal is put on the DIR pin (i.e. High). "The data sheet does not say if a high on the DIR pin makes the stepper motor rotate…
Part Number: DRV8436 Hi team,
I wanted to know regarding the Supply voltage range parameters and the ability to work into Abs Max.
Our application has rated + 48V motor power supply voltage, without particular fluctuations by the power supply. For reasons…
Part Number: DRV8436 there is a new datasheet from DRV8436. i saw that open load detection has been dropped. my problem is that the line nFault is set when i change the direction of the motor. the error message remains set, but i can still drive the motor…
Part Number: DRV8436 Hi all
I did not find the same.
Where can download the DRV8436 EVM GUI, we didn't find it on ti.com. Customers need GUI.
Best Regards, Ishiwata
Part Number: DRV8436 Hello,
We have just bought the evaluation board for the DRV8436E (DRV8436EEVM) but I can't find the SW on ti.com
The user guide says: "Download the installable DRV843x_x.x.x_installer_win.zip file." but there's no link to the…