Part Number: DRV8701 Hello, I would like to know more details about the offset voltage of the current sense amplifier.
The datasheet quotes the value of 50 mV with maximum of 250 mV. This seems like a rather large range, and I would like to know which…
Part Number: DRV8701 When using the DRV8701 to drive the upper and lower MOSFETs (applied to the drone motor board), one arm has three sets of MOSFETs (one set of MOSFETs includes the upper and lower tubes), one of which occasionally burns out when the…
Part Number: DRV8701 hello
my project is jusing the DRV8701ERGET which is end of life/ OBSOLETE and we want to find alternative without any hardware changes can you please assist
thank you
Guy C
Part Number: DRV8701 I am observing dV/dt-induced parasitic turn-on of the low-side MOSFET (cross conduction) during switching, exactly as described in section 2.2.3 of the "Understanding Smart Gate Drive" Document. Specifically:
When running at 50…
Part Number: DRV8701 Tool/software: Dear teams,
When using DRV8701P to drive a DC brushed motor and measuring the GH pin with an oscilloscope, an abnormal waveform was observed.
PWM control frequency 20KHZ, powered by DC24V. The test waveform is as…
Part Number: DRV8701 Hi,
In attached DRV8701 TI PSPICE output waveform with all default settings ,18V 6mA profile Vgh2 is expected to be 0V but it is High for some time.
Part Number: DRV8701 We have configured a BDC motor drive circuit using the DRV8701P and four TSM120N06LCP MOSFETs.
However, when the motor is initially driven, an EMI radiation failure occurs, which appears to be caused by a current regulation response…