Part Number: DRV8702-Q1 Hello;
Q3 2021 we replaced the DRV8702-Q1 in our design by an other motor driver because of availability.
Because of EMC reasons we want to change it back.
At TI online shop the maximum order quantity of the DRV8702-Q1 is 50.
…
Part Number: DRV8702-Q1 Dear TI-Team,
for our project I would like to drive two single directional brushed-DC motors independently with one DRV8702.
Is this possible and if yes, how can I control both motors via IN1/IN2. Is the VDS(OCP)-protection still…
Part Number: DRV8702-Q1 Hi,
Looking to use an H bridge for polarity control of current going through a TEC element and need to maintain a DC current so would not be using an PWM modulation (need to keep at 100% duty cycle and only change the direction…
Part Number: DRV8702-Q1 My customer found the description about spread spectrum function in DRV8702-Q1 datasheet. But there is no instruction about how to configure this function. Could you help explain and instruct customer how to configure?
Part Number: DRV8702-Q1 Hi,
I have a DRV8720 conntected to 4x CSD18510 FETS. My motor is a brushed DC motor powered from 24V.
The driver is operating in Mode=High-Z where I am supplying the PWM directly.
In the picture below I have:
1. Green = Motor…
Part Number: DRV8702-Q1 Other Parts Discussed in Thread: DRV8706-Q1 , DRV8245-Q1 Hello,
I am an FAE for a distributor that handles TI products. I am researching the product in the specifications below. I prefer the DRV8702-Q1 and DRV8706-Q1. However, I cannot…
Part Number: DRV8702-Q1 Hello team,
My customer encountered the following problems when using DRV8702.
The the Amplifier Gain of DRV8702 is 19.8 only when 60mV<Vsp<225mV. They want to know, when the Vsp voltage is less than 60mV, what is the value…
Part Number: DRV8702-Q1 Other Parts Discussed in Thread: DRV8705-Q1 , DRV8714-Q1 I am planning to use the motor driver in independent PWM mode. PWM frequency of both the motors are 20KHz. Maximum current of 1st motor is 1A and 2nd motor is 7A. I will be…
Part Number: DRV8702-Q1 Other Parts Discussed in Thread: DRV8705-Q1 In the Datasheet it seems to recommend Bulk capacitors on the VM pin and the high side of the FETs. In my circuit I am intending to add some impedance between VM and the high side FETs…
Part Number: DRV8702-Q1 Hi team,
My customer has two questions with DRV8702-Q1. Would you pls help check and share your comments?
1. Do we have the leakage current data of SHX for DRV8702-Q1? It is a required information from OEM side. They needs to know…