Part Number: DRV8703-Q1EVM Other Parts Discussed in Thread: DRV8703-Q1 , Dear Support team,
Our customer will use DRV8703-Q1 in their application. They are using the DRV8703-Q1EVM to check the occurrence of a flag when a fault is detected. Please tell…
Part Number: DRV8703-Q1EVM Other Parts Discussed in Thread: DRV8703-Q1 Hai,
Thanks for responding my previous queries.
In the DRV8703-Q1 EVM board the H-bridge connected to the driver IC seems like operating in the HIGH SIDE DRIVE configuration. The…
Part Number: DRV8703-Q1EVM Hai,
Thanks for responding my previous forums.
As per your suggestion I removed resistors between micro and driver IC of IN1 and IN2 pins, because I want to drive the motor with external micro by providing PWM to IN2.
…
Hi Huan,
A common reason UVLO can occur is when large or varying loads draw large amounts of current which can cause the supply voltage to dip. Having a sufficient amount of bulk capacitance on the supply voltage will reduce the amount the supply voltages…
Part Number: DRV8703D-Q1 Other Parts Discussed in Thread: DRV8703-Q1 , DRV8703-Q1EVM The DRV8703-Q1 datasheet clearly specifies the SPI mode configuration (mode 1).
After hours of debugging our board, we decided to probe the D RV8703-Q1EVM dev board…
Hi Huan,
Yes the PWM is usually generated by a microcontroller. This is required only if you'd want to have a PWM speed control. Applications that don't need speed control can be controlled by SPI IN1 and IN2. The DRV8703 does not have internal PWM…
Part Number: DRV8703D-Q1EVM Other Parts Discussed in Thread: DRV8703-Q1EVM , DRV8703-Q1 , DRV8706-Q1 , DRV8705-Q1 DRV8703D-Q1EVM eval board it says bi directional motor control on the text but I see only 2 FETS. how can it do forward and reverse?
…
Hi Tommy,
Understood. To be very positive that there will not be any problems with the frequent current direction changes, I recommend testing it on one of our evaluation boards (DRV8703-Q1EVM). Plus it would be good to drive your load with our eval…
Part Number: TIDA-01421 Other Parts Discussed in Thread: DRV8703-Q1EVM , INA240 Hello again!
I am making this thread in continuation to the old thread e2e.ti.com/.../889204 (TIDA-01421: Obtain a signal when driving motor with relays)
Since my last…