Hi Rohan,
Thanks for sharing the requirements. The DRV8462 in DDW package can support up to 10 Amps IFS motor current and support up to 65 V operating voltage. The EVM for this device is DRV8462VEVM. This package DDW requires external heatsink for power…
Part Number: DRV8711 Tool/software: Is it acceptable to connect SLEEPn directly to the V5 supply voltage. I do not need the sleep function and want the chip enabled all of the time. Thanks...
Part Number: DRV8711 Other Parts Discussed in Thread: , , CSD18531Q5A Tool/software: Hi,
My company has ~800 stepper driver boards built with DRV8711s & CSD88537NDs. They have worked pretty well for us at 24V and 1-2A with one pre-driver fault every…
Part Number: BOOST-DRV8711 Other Parts Discussed in Thread: DRV8711 Tool/software: Hi,
One of our customers facing an issue with BOOST-DRV8711 on the board.
I am reaching out regarding a technical issue I'm facing with the DRV8711 booster board in our…
Part Number: DRV8711 Tool/software: I am troubleshooting a non-functioning PCB that is a mature design and normally works but this particular board is having it's fault pin LED light up. I checked the status register using some built in debug software…
Part Number: DRV8711 Tool/software: Dears,
The customer used DRV8711 to drive the stepper motor for 2000 steps and then slowed down and stopped normally. At the end, sets full-scale output current (TORQUE register set to 0x20) .After about 5 seconds…
Part Number: DRV8711 Tool/software: What is the difference between the following part DRV8711DCP & DRV8711DCPR.
What denotes R?
is this package difference? If yes, please share evidence doc
Please clarify
Part Number: DRV8711 Tool/software: Hi experts,
This is Skylar responsible for GREE. Here are the questions for DRV8711.
Does DIR pin have any requirements on the signal level when changing directions? If we want to change the direction and the DIR pin…