Part Number: BOOST-DRV8711 Other Parts Discussed in Thread: UNIFLASH , MSP430G2553 Hi Team,
Customer has following questions need your help.
Download the latest version of the GUI Composer Runtime to initially run the BOOST-DRV8711 GUI: You must register…
Part Number: DRV8711 Other Parts Discussed in Thread: DRV8461 Hello,
I have a customer whose application is a stepper motor drive, and he says that he is getting a distorted current waveform whenever the motor goes above 100-150 RPM. The waveform is pasted…
Part Number: DRV8711EVM Other Parts Discussed in Thread: DRV8711 , HI,
A my account has below question about DRV8711. Pls kindly help check them.
How does the register setting of IDRIVEP&IDRVEN impact the voltage noise amplitude on SCLK pin ?
When…
Part Number: DRV8711 Hi experts,
Nice to e-meet you! This is GREE FAE Skylar.
There is a question from GREE about DRV8711. The phase current parameter of their motor is 4A. But when they tested their board performance, if they want to run the maximum…
Part Number: DRV8711 Questions:
How to achieve a low noise performance of stepper?
What impacts noise of a running stepper?
Which drv8711 driver configurations impact noise?
How to achieve a minimal vibration performance of a stepper?
What causes…
Part Number: DRV8711 hi
a my account wants to know if different SMPLTH value impacts real Back EMF value of motor when the bit values in STALL register, including SDTHR,SDCNT and VDIV, are same?
2, Is there any detailed material to address how the…
Part Number: DRV8711 Hi Team,
DRV8711 drives the stepper motor to generate severe heat. The voltage is 48V. The motor has a peak driving current of 1A, and even after stopping, there is still coil current, causing the motor to sizzle.
Regards,
Annie
Hi Grzegorz,
Thanks.
Grzegorz Pelikan said: That ringing usually rises with output current. You can try to capture max. amplitude of ringing by setting trigger on BISENP and slowly adjusting it until oscilloscope stops to trigger. If captured max. ringing…