Part Number: DRV8711 Other Parts Discussed in Thread: TM4C1294NCPDT , , DRV8889-Q1 Hi.,
I am using TM4C1294NCPDT Microcontroller, and using DRV8711 for controlling stepper motor. We command the motor for moving one position to another position.In that 2nd…
Part Number: BOOST-DRV8711 Other Parts Discussed in Thread: MSP-EXP430G2ET , DRV8711 , UNIFLASH , MSP430G2553 , DRV8711EVM Hi,
I have a BOOST-DRV8711 with a MSP-EXP430G2ET. I am following the manual of the BOOST-DRV8711 but I cannot get past part 4.3 in the…
Hello Tom,
Thanks for the update. I did understand the constraints you had getting all four channels, really appreciate you providing all the requested captures. I tried to identify the root cause for your issue from the captures you sent.. The DRV8711…
Part Number: DRV8711 Hi.,
I need the favor from you.
I'm using DRV8711 for my project.My requirement is to stop the stepper motor few seconds in running sequence.(Stall detection)
I'm using 5 positions of stepper motor. In the second position , …
Part Number: DRV8711 Hi,
DRV8711 is used to drive a stepper motor; the VM voltage is 24 VDC. APDF/BPDF was detected when the motor was driven.
Conditions for APDF/BPDF.
・Whether or not the gate-source voltage exceeds 1 V 2.2 us after the current is sourced…
Part Number: DRV8711 Hi,
We have used stepper motor for one of our application. So we choose the DRV8711 driver IC. But we powerd up and connect the motor at that time drive goes OCP and UVL. may i know the reason for these errors.
We used the shunt of…
Part Number: DRV8711 Other Parts Discussed in Thread: DRV8434 , DRV8955 Hi,
Usually the motor to be connected will have a winding rating of minimum 150 mA. so i am looking for the peak or continuous RMS current per channel driver can output.
I am only…
Part Number: BOOST-DRV8711 Hi,
Good Day.
I have this module "BOOST-DRV8711" and I have connected the stepper motor to it and connected the Arduino uno board via SPI.
I have programmed the uno board with the program of providing the step signal…
Part Number: DRV8711 Hi Team,
I need help with the question below:
If A1HS and A2LS are enabled and the MOSFETs are energized what should be measured across the Coil A.
This part is used as a driver for a stepper motor with the VM is set to 24 VDC
Thank…