Part Number: DRV8711EVM Hi Team,
The D3 light flashes after the USB is connected, and the D2 light does not light up after 24V is powered on. The wake-up does not work, the software cannot control.
Thanks,
Annie
Hey Jacob,
Thanks for the resources.
To reply:
The motor I am currently using is the WO-5718L- 01P - RO LIN ENG.
Resistance 1.1 Ohms/Phase
Inductance not known
I am using TI's DRV8711EVM board: https://www.ti.com/tool/DRV8711EVM
Additional questions…
Part Number: DRV8711EVM Other Parts Discussed in Thread: DRV8711 , Hi I have a requirement to drive 24V-300W Bi-polar stepper motor to drive.
Can i use DRV8711 as a reference with change in MOSFET & Current sense resistor to full fill my requirement?…
Part Number: DRV8462EVM Other Parts Discussed in Thread: DRV8462 , DRV8711EVM , Hello.
Can someone from TI please tell me if the above part number would support the following stepper motor? I would like to find the correct platform EVM to develop my application…
Part Number: DRV8711EVM I hooked up a new DRV8711EVM and ran it in forward and reverse a few times. After it was sitting idle for a minute or so I noticed a large current draw - approximately 10 amps and I shut off the power supply. I smelled something…
Part Number: DRV8711EVM Hi Ti,
Can I use other programming software, like Labview, to communicate with this module? We want to synchronize the motor with our system. GUI seems unable to do that.
Best regards,
Siyuan
Hi Igor,
More information would be helpful to understand the problem statement accurately. Were you describing the status of the driver outputs after power on and enabling the motor using ENBL = 1 in the CTRL register -or- was it soon after power on …
Part Number: DRV8711EVM Hi,
After doing the reset in GUI, all registers getting its default state. But after the reset cleared in GUI, all the bits of registers hold 1 , including status register but fault LED is not blinking.
Followed steps:
Step …
Part Number: DRV8711EVM Other Parts Discussed in Thread: DRV8711 Dear team,
I am using DRV8711 for stepper motor control project. I found that the resistor connected between MSP and DRV8711 in the reference design is 0.
RES, 0 Ω, 1/10 W, 0603, SMD R6, R7, R8…
Part Number: DRV8711EVM Other Parts Discussed in Thread: MSP-FET , MSP430F2617 , MSP-EXP430F5529LP , DRV8704 , DRV8711 , BOOST-DRV8711 Hallo,
we plan to make stepper tests with the DRV8711EVM board.
Is it possible to change the program and flash it?
What is…