Part Number: DRV8714-Q1 We are trying to use a DRV8714-Q1 in H-Bridge PH/EN Mode.
When not driving the motor, we want the outputs to be both low - hence the gates for both low-side FETs must be high.
We are finding instead when IN1/IN2 are low, both…
Part Number: DRV8714-Q1 Tool/software: Hello Team, is there any concern to use this part in a 3V3 environment? Means connecting DVDD to 3V3 and can drive all other logic with this levels (i.e. SPI, Digital In/Out). Many Thanks Josef
Part Number: DRV8714-Q1 Hi Team,
We have a questions about the DRV8714-Q1 PON threshold.
-> For Volvo ZCU RFQ.
From the DS that the VPOB_OV is 30.5V, from my understand that we need to make sure IC itself will not be damaged when POB happen so we…
Part Number: DRV8714-Q1 Tool/software: Hi team,
Here is a new question about DRV8714-Q1.
Customer found that the GH1 is always high after a DVDD cycle from 5V->2.5V->5V。 Shown as below: CH1 is PWM input, CH2 is the GH1.
Support need: What is the…
Part Number: DRV8714-Q1 Tool/software: Hello,
can you please explain VGS drive and VDS monitor blanking time vs. VDS overcurrent monitor deglitch time? Do you have an example waveform for VDS_OCP function and mark the different times?
BR,
M…
Part Number: DRV8714-Q1 Tool/software: Hi Team,
we are doing EMC, Signal integrity and power integrity for our PCB's. we are using the motor driver DRV8714SQRVJRQ1 in our project.
So, here we are in required IBIS model for the simulation. kindly…
Part Number: DRV8714-Q1 Tool/software: Hello,
When DRV8714-Q1 is used as H-Bridge, I would like to know that how ~5.3V is appearing at SH1 and SH2 during offline diagnostics in the case of no fault.
Thanks,
Sathish.
Part Number: DRV8714-Q1 Tool/software: Hi team,
Is there a failure mode in the DRV8714 and DRV8703 chips that will cause the diagonal MOS of the H-bridge (such as the left high side and the right low side) to turn on at the same time?
This is a requirement…
Part Number: DRV8714-Q1 Tool/software: Hello team.
I would like to know what the path will be when 5V is applied to the NSLEEP/DRVOFF/NSCS terminals while PVDD and DVDD are open.
As ECU of the failure mode check, we check the behavior of the IC…
Part Number: DRV8714-Q1 Tool/software: Hi All ,
Requesting DRV8714 register configuration for Hbridge activation using PWM . I have hurdle in achieving the below status