Part Number: DRV8714S-Q1EVM Other Parts Discussed in Thread: DRV8714-Q1 Tool/software: Hello, Currently I try to integrate DRV8714S with DSPIC33CK256MP508. I use MPLAB X IDE for code development, but I strill struggling with the code especially to read…
Part Number: DRV8714S-Q1EVM Tool/software: I have a question about the marked sections. Could you please provide the connector pitch size & that screw terminal wire size
Part Number: DRV8718S-Q1EVM Tool/software: Hi team,
Our customers are designing external circuits for the DRV8718 and DRV8714 and are experiencing the following issues: 1, DRV8718 and DRV8714 are 56pin, in the design need to design 57 pin for reservation…
Part Number: DRV8714S-Q1EVM Hi team,
Here's an issue from the customer may need your help:
Assume two half-bridges are used to set the PWM complementary outputs as follows:
Half Bridge 1 setup: Set HB1_PWM to 00B according to Table 8-4 below, that…
Part Number: DRV8714S-Q1EVM We have a motor drive system that plan to use FRV8714S-Q1, now development is ongoing, due to reduce development timing, is any code example can be referred like register initial config?
Part Number: DRV8714S-Q1EVM Hello E2E,
Our customer tries to verify some monitoring strategies with the DRV8714S Demo board. They short the Motor and set register filter time to 4us and VDS = 0.6V and found the current will be limited to 90mA and report…
Hey Darshan,
Se the BRG_MODE bits to 0b10
BRG_MODE is in IC_CTRL1, so to spin the motor you'll need
EN_DRV=1
EN_OLSC=whichever, 0
BRG_MODE=10
LOCK=011b (unlocked)
CLR_FLT=whichever, 0
Thus IC_CTRL1 = 0b10100110
Do you have an EVM? This will be…
Hey Ling,
ling xinjie said: Why Vdrain ≠ Vsh1?
For that let me refer with a coworker who is more familiar with this device, give us a day.
Make sure you have the required external components for this part matching the datasheet. Do you have an EVM you could…
Part Number: DRV8714-Q1 Other Parts Discussed in Thread: DRV8714S-Q1EVM Please tell me the voltage that can be applied to nSCS under the following conditions.
PVDD=12V DVDD=OPEN nSLEEP=Lo
From the perspective of the SPI communication line, I think that nSCS…