Part Number: DRV8718-Q1 Hi expert,
My customers plan to use DRV8718-Q1 as the MRC controller, they plan to use 2xDRV8718-Q1 to controll 8xH-Bridge achieving 10kHz swtiching frequency for each H-Brdige with same SPI network and seperate nCS signal. …
Part Number: DRV8718-Q1 Hi Team,
My customer is using daisy chain. They said they found sometime, they can not read data from SPI, and the devices can not run the motor at the same time.
They have multi daisy chain on board, some of them with 2 devices…
Part Number: DRV8718-Q1 Hi team,
My customer wants to know the maximum SPI speed for DRV8718-Q1, is 10M can be accessible? If not, what is the maximum value?
BR,
Daniel
Part Number: DRV8718-Q1 Hello,We use the MD026B development board jumper to connect to our own MCU debug DRV8718, where the DVDD, AREF, nSLEEP pins input 5V voltage, PVDD pin input 12V, control register configuration as shown below, we want to use OUT1…
Part Number: DRV8718-Q1 DRV8718 is used to drive H-Bridge and internal current sense amplifier(CSA) is for inline current sampling.
The calculation formula is Vout=(V+ - V-) x GAIN +VREF
GAIN=20, VREF=AREF/2=2.5V
If (V+) - (V-) = 0.08V , CSA Vout…
Part Number: DRV8718-Q1 Hi Team,
When DRV8718 not drive MOS FET and our offline diagnostic not open, if there happen MOS FET short to ground, whether our DRV8718 OCP function will work normal or not?
Hi Shahajahan,
Thanks for your post.
shahajahan m said: How can I sense normal operating current and detect stall current using this IC?
What is the normal operating current and stall current for the brushed DC (BDC) motor in your application, either…
Part Number: DRV8718-Q1 Dear TI experts,
Can I get FMEDA document of DRV8718SQRVJRQ1 to check FIT data regarding to ISO26262 standard?
I cannot find the document on TI.com product page.
Best regards,
Chase
Part Number: DRV8718-Q1 Other Parts Discussed in Thread: DRV8714-Q1 , Hi Expert,
Have a nice day! I have question need your professional support:
For DRV8718-Q1/DRV8714-Q1, I find difference between power supply of LS Amp:
For DRV8718H-Q1, DRV8718S…
Part Number: DRV8718-Q1
Tool/software:
Hello Colleague
In my application, the offset setting is Aref/8 = 0.625V. That means I can read the voltage 0.625V from SO pin when the load current is 0.
Actually, when the external motor is stop, the shunt…