Part Number: DRV8718S-Q1EVM Hello,
I am using a DRV8718s evaluation module to drive a coil through PWM. I configured the driver for IN1 and IN2 to drive the high sides of half-bridges 1 and 2, respectively. The coil leads are connected to half-bridge…
Hi Imrich,
There's one way to verify if the EVM and its onboard MSP430F2617 are functional if you have the MSP-FET debugger with you.
Connect the MSP-FET JTAG connector to J3 observing pin1 orientation.
Connect the MSP-FET USB to a computer. …
Part Number: DRV8718S-Q1EVM Hi TI expert:
The SPI configuration of the MCU is as follows:
MSB, 1000000MHz, CPOL=0, CPHA=1.
I want to read the value of the status register of the DRV8908 through SPI. The following table shows the data received by…
Part Number: DRV8718S-Q1EVM Hello TI Support Team / Forum,
I am working with the DRV8718S-Q1 motor driver and would like guidance on monitoring motor current via the integrated current sense amplifier. Specifically, I have the following queries:
…
Part Number: DRV8718S-Q1EVM Hi,
As shown in the figure below, the MCU is externally connected with three DRV8718 devices in the daisy configuration.
I wanted to write the value 0x80 into the register IC_CTRL1(addr =07) of the first device, and then…
Part Number: DRV8718S-Q1EVM Tool/software: I was running some tests with the DRV8718S-EVM, and everything was working fine when using the GUI. After disconnecting the PCB from power, I placed a pin header onto the PCB (just to measure the physical dimensions…
Part Number: DRV8718S-Q1EVM Tool/software: Hello Team,
On the DRV8718S-Q1 I'm trying to monitor the current with CSA, My motor is connected to the output NC/OUT1 & OUT1/OUT2 of the EVM. I'm able to control the motor with a PWM in both directions.
…
Part Number: DRV8718S-Q1EVM Tool/software: Hallo,
I'm currently waiting to receive the EVB but I wasn't able to find the detailed contents of the shipping box.
Is the power supply to be connected to VBAT (connector 8 of fig 2.7 EVB user's guide) coming…
Part Number: DRV8718S-Q1EVM Tool/software: Hi team,
Our customers are designing external circuits for the DRV8718 and DRV8714 and are experiencing the following issues: 1, DRV8718 and DRV8714 are 56pin, in the design need to design 57 pin for reservation…
Part Number: DRV8718S-Q1EVM Other Parts Discussed in Thread: DRV8718-Q1 , Hello sir ,
1)I am using DRV8718-Q1 EVM board , am also changing the PWM value of input but there is no output coming . Please tell me how can i use this EVM board .
2) There…