Part Number: DRV8801-Q1 Other Parts Discussed in Thread: DRV8801 Hi all, The datasheet described that "When switching from low to high, the user should allow a 1-ms delay before applying PWM signals. This time is needed for the chargepump to stabilize…
Other Parts Discussed in Thread: DRV8801-Q1 , DRV8801 Hello,
I have a question about DRV8801-Q1. What is the thermal shutdown temperature(min) ? If you have a graph, which shows time vs thermal resistance, could you please provide it? The following…
Other Parts Discussed in Thread: DRV8801-Q1 , DRV8801 , DRV8801A-Q1 Hi, Team,
I have a question about "nFault" of DRV8801-Q1.
Customer wants to use it on VBB=9V with Fault indicate function.
However I know DRV8801 has VBBNFR is 12V typicaly. …
Hi Hsu,
The links to the latest datasheets are:
DRV8801-Q1 (SLVSAS7B) http://www.ti.com/lit/ds/symlink/drv8801-q1.pdf
DRV8801 (SLVS855J) http://www.ti.com/lit/ds/symlink/drv8801.pdf
Hi Kei, using a larger inductor should allow you to use a larger capacitor and not hit OCP. Does increasing the capacitor improve the noise? Maybe you could try to keep increasing it.
Best regards,
RE
Part Number: DRV8876-Q1 Other Parts Discussed in Thread: DRV8801-Q1 , DRV8874-Q1 , DRV8874 , Hi team
How should we control BMD motor driver as BLDC with external hall sensor?
Is DRV8776-Q1 or DRV8874-Q1 possible to use as BLDC motor driver instead…
Part Number: DRV8876 Other Parts Discussed in Thread: DRV8801 , DRV8801A-Q1 , DRV8801-Q1 , DRV8816 , DRV8874 , Hi there,
My team is interested in utilizing one of the following parts:
DRV8801
DRV8801A-Q1
DRV8801-Q1
DRV8816
DRV8874
DRV8876…
Part Number: DRV8876-Q1 Other Parts Discussed in Thread: DRV8801-Q1 , Hi Expert,
I need a Q1 level(use for auto) motor driver device to drive the DC motor in electronic lock.
I only need a +12V output to open the lock motor, and a -12V output to…
Other Parts Discussed in Thread: DRV8801-Q1 , DRV8870 Hi,
I would like to know if the device is protected for short to ground on all pins, that is a requirement needed for automotive application.
For example in DRV8801-Q1 datasheet we say short to…
Other Parts Discussed in Thread: DRV8801-Q1 , DRV8802-Q1 , DRV8802 , DRV8828 I'm FAE of distributor,I support Automotive customers in Japan.
Customers want DC motor driver, request spec is max 40V,3A output.
They feel DRV8801-Q1 is not enough max…