Part Number: DRV8801A-Q1 Other Parts Discussed in Thread: DRV8801 Hi, if we power the DRV8801 from 24V, would the output be able to drive +-/12V?
Thanks,
Jeramie
Part Number: DRV8801A-Q1 Other Parts Discussed in Thread: DRV8873 , DRV8143-Q1 , DRV8873-Q1 Hi team!
The customer wanted to use DRV8801A-Q1 to provide single direction current, such as using PWM control OUTA upper switch, and OUTB lower switch is always…
Part Number: DRV8801A-Q1 Hey Team,
In old Datasheet (SLVSC79C), the Charge pump voltage is mentioned as Vbb+7 whereas in new Datasheet (SLVSC79D) it's mentioned as Vbb+17.
Is this a change or typo?
Old:
New:
Best, Dajon McGill
Part Number: DRV8801A-Q1 Hi Team,
With the DRV8801A-Q1 in automotive applications is there any protection devices we recommend when using off battery?
Big electrolytic? TVS?
Thanks,
David
Part Number: DRV8801A-Q1 Hi
Ti Team,
I need a Ibis model for above part number DRV8801A-Q1 for my SI / PI Simulation
please provide me for my personal mail.
let me any further details is required.
Thanks & Regards
Sathya KR
Part Number: DRV8801A-Q1 Other Parts Discussed in Thread: DRV8703-Q1 , DRV8801 , Can i drive an external FET for reverse battery protection using the charge pump of the DRV8801A-Q1? There is no information in the datasheet about the charge pump. In the…
Hi Jin-Suk,
It is difficult to predict if there is a problem. Care should be taken when trying this the first time.
When the motor is powered, the 12V will pass through the body diode to VBB. If VBB is used to power the remainder of the board, then…
Part Number: DRV8801A-Q1 Other Parts Discussed in Thread: TINA-TI Tool/software: TINA-TI or Spice Models Hello All,
Could you please share some link or some suggestion to do simulation on this driver in Pspice or Simetrix.
Part Number: DRV8801A-Q1 Hello Team,
Kindly help me with the calculations required to find the value of Inductor which should be kept in series with the MOTOR winding between the H-Bridge outputs. This Inductor is used to limit the inrush current along…