Part Number: DRV8806 Hi Team,
Use the DRV8806 to drive the stepper motor, please see the schematic and motor spec as follows:
By checking the waveforms for the four outputs A, -A, B, -B t hrough the oscilloscope, it can be seen that there is a large overshoot…
Part Number: DRV8806 Other Parts Discussed in Thread: DRV8411A , DRV8461 , DRV8452 , DRV8462 , DRV8434A , DRV8434S , DRV8889-Q1 , DRV8711
Need to find a driver for 28BYJ-48 stepper motor, which driver will be most suitable. I need the driver with stall detection…
Part Number: DRV8806
Hi team,
Here's an issue from the customer may need your help:
Customer uses 3 DRV8806 units for cascaded output control loads and can now control the OUT port but with the following issues:
1) Currently only 12ohm resistor and…
Part Number: DRV8806 Other Parts Discussed in Thread: DRV8873 , Hi,
Customer search for solenoid drivers to apply to the rice cooker.
Please recommend a product that meets the conditions.
* Solenoid driver specification
Input voltage: 12V to 24V.
Driving…
Part Number: DRV8806 Other Parts Discussed in Thread: DRV8904-Q1 , DRV8906-Q1 , DRV8908-Q1 , DRV8860 , DRV8706-Q1 HI team,
My customer is looking for Inductive Load driver solution.
1)The constant current requirement is 1.5A, transient peak current requirement is 3.5A…
Part Number: DRV8806 Hi team,
My customer wants to evaluate the DRV8806 in the system. The structure is below. The green side is the board. The Vm is powered by the board 24v. The inductor pull up side is connected to another 24v. The other side of the inductor connect…
Part Number: DRV8806 Dear Team
Since we book the incorrect part number, could you help cancel salesaorder,T01540279 , part#DRV8806PWPR 2k
thank you so much
Part Number: DRV8806 Other Parts Discussed in Thread: DRV8803 , DRV8804 , DRV8804EVM Hello,
My customer wants to evaluate the DRV8806 but there is no longer an EVM for it. The DRV8803/4/5 EVM uses a 20 pin package which doesn't seem to be available for…
Part Number: DRV8806 Hi Team,
The customer is experiencing below issue and needs your help.
1. How to solve the leakage current during DRV8806 control? For example, when the DRV8806 is powered on but not turned on, D11 and D15 will have weak light. When…