Part Number: DRV8908-Q1 Other Parts Discussed in Thread: DRV8808 Dear expert,
Can I connect two output together to drive one 2A H-bridge load with one DRV8908?
Below two current is 4A in this case , right?
"Continuous supply current (VM pins combined…
I have a motor/dc-dc control board. I cannot find the datasheet for the PWM Power Driver IC. It is a 48 pin HTSSOP. Could you please help me find the datasheet. Pinout does not match DRV8808. The markings on the chip are: 95AKRPTC/SC76025/1825-0350 (First…
Other Parts Discussed in Thread: L293 , DRV8808 , DRV8837 , DRV8838 , TLV61046A Hi, i am working with battery powered water flow controller project and i listed the hardware part my design in below,
1. 6V rechargeable battery,
2. IR Transceiver,
3. 8pin microcontroller…
Other Parts Discussed in Thread: DRV8800 , DRV8811 , DRV8812 , DRV8821 , DRV8823 , DRV8809 , DRV8808 A student is developing a solar energy trailer with MCU-controlled sun tracking feature and wants to know how to use TI parts to enable his project. Here's his…