Part Number: DRV8811
Tool/software:
The driver works driving a little step motor in full-step mode, the max current is configured to be <500 mA using sense resistors of 0.4 Ohm and Vref 1.55 V, Vcc is 3.3V. We experienced similar failures (shortcircuit…
Part Number: DRV8811 Hi,
We are having a DRV8811 based PCB that driving a stepper motor which is used to control valve movement. Recently we are seeing some PCB failures. After some debugging and it is found the DRV8811 has been failed due to some…
Part Number: DRV8811 With the supply chain issues, we have been buying what we can get in the market. we have been having field issues regarding with this driver and reading through the forum I ran across a discussion that sounds exactly what we are seeing…
Part Number: DRV8811
HI Expert,
My customer find the peak current on both AOUT and BOUT.
1. Could you please let me know the reason of this peak current?
2. Also, could you please let me know the reason of difference peak current between AOUT…
Part Number: DRV8811 Hi Expert,
VM UVLO for rising is 6.7V(typ) and 8.0V(max) from datasheet.
Could you please let me know the VM UVLO value for falling ? Is it same value?
Also, please let me know the minimum value. (There is no problem with…
Part Number: DRV8811 Other Parts Discussed in Thread: DRV8880
Hello,
Above is a shot of the issue with my motor driver.
It is a snapshot of two current probes across a coil. Using an FFT sound analyzer on my phone, I hear 850Hz which matches…
Part Number: DRV8811 dear
My customer fihd that DRV8811 drive motor appear speed too fast, phenomenon just show below picture
note: 频率 means frequency
It appears sometimes ,about probability of 1/15
AOU1 AOUT2 BOUT1 BOUT2 wave shows as above…
Part Number: DRV8811 Hi expert,
Could please give me your advice for root cause of the following difference between AOUT and BOUT current.
-In the waveform, the current is insufficient on the High current side, and it should be 0A on the Low…
Part Number: DRV8811 Hi Expert,
The step angle of the step#2 for 1/8step is 11.325 in datasheet table2 .
Is it typo? I think, it is 11.25 from around values.
Also, which is correct actual behavior?
1) Actually, outputs will be set Aout=98…