Part Number: DRV8813 Dear Sir/Mdm, We do face some issue with our latest production 100% testing process with the latest delivery of DRV8813PWPR where we purchased from Arrow Electronics.
I.e. the previous release batch of Part were working and perform…
Part Number: DRV8813 Hi All,
I have a question about the DRV8813.
I would like to reset with the nRESET pin after the protection circuit operates. How long after reset can I enter PHASE/ENBL?
Best Regards, Ishiwata
Part Number: DRV8813 Greetings!
I'm trying to configure the DRV8813 for PWM control of a PMDC motor, but I don't think I fully understand the operation of this chip from the datasheet. According to the datasheet, the A-phase inputs are for setting output…
Part Number: DRV8813 Hi team,
My customer is using DRV8813 to drive a stepper motor. VMA and VMB are combined together to 24V. VMA has a 1000pF cap to GND and VMB has a 1000pF cap to GND. When the motor is in operation, we found there are some spur…
Part Number: DRV8813 Other Parts Discussed in Thread: DRV8881 , DRV8426 Hi All,
I have a question about the DRV8813.
How much does the accuracy of the output current change depending on the set voltage of VREF?
The DRV8881 data sheet had the following…
Part Number: DRV8813 Hi All,
The DRV8813 drives one DC motor.
How should I set the unused terminals? For example, please tell me how to terminate BPHASE / BENAB for input, BOUT1 / BOUT2 for output, and ISENB.
Best Regards, Ishiwata
Part Number: DRV8813 Dear Specialists,
My customer is evaluating DRV8813 and has a question.
I would be grateful if you could advise.
---
According to the datasheet, nSLEEP response time is described 1ms as sleep mode to inactive (nSLEEP L to…