Hi Rick,
I did finally have some success after running the program in XP compatibility mode. After completely deleting and re-installing the slv342 version, I found that there was no more setup.exe folder, but the readme says to use CPG004-5_DRV88xxEVM_R1p1…
Part Number: DRV8825EVM Other Parts Discussed in Thread: DRV8825 Hi
Our customer are going to evaluate DRV8825 with ERV8825EVM.
Then I have a question about configuration of EVM. What is the R11 and R12 for between DRV88xx and MSP430?
Should…
Part Number: DRV8825EVM Other Parts Discussed in Thread: DRV8825 Hi,
I am using DRV8825 evaluation module , whenever i use DAC input for the VREF there is a lot of noise in stepper motor and the expected speed is not achieved.Tried slow and fast decay…
Hi Mario,
Sorry for the delay getting back to you. As mentioned, the EVM has approximately 80 sq inches of 2 oz copper while the thermal calculator uses 8 sq inches of 1 oz copper (effectively 20 times the thermal mass).
Please refer the LINK , which…
Other Parts Discussed in Thread: DRV8825EVM Dear Sir ,
I have just started to use the TI make DRV8825EVM and connected to the stepper motor. Using the application program i was able to connect (communicate) and then i configured the settings as per…
Other Parts Discussed in Thread: DRV8825 , DRV8825EVM Hello motor drivers forum, I had to write my own trajectory generator (the S-curve) that uses DRV8825 IC. I programmed the DRV8825EVM from CCS 5.3 using MSP-FET430UF, but ran into the motor "growling…
Other Parts Discussed in Thread: DRV8825EVM , DRV8825 Hi,
I just started using DRV8825EVM ...I have no idea how to write a code and how to interface a program written in CCS4 with DRV8825EVM , to control stepper motor....can u please help me?????
Hi Vasuki,
Thank you for your question.
Vasuki Tanuja Pulikonda said: Can I use this stepper motor driver with an Arduino Uno to control a stepper motor?
The DRV8825 is a very popular general purpose bipolar stepper motor driver with tons of examples…