Part Number: DRV8828 Hello Team,
Good day.
My customer, using a DRV8828PWPR motor controller with a 33GB-520 DC motor. VM is 12V, VREF is 3.3V, directly connected to an Arduino 33 IoT's 3V3OUT pin. V3P3OUT (pin 15) is bypassed to the ground. Since…
Part Number: DRV8828 Dear Specialists,
My customer is considering DRV8828 and has a question.
I would be grateful if you could advise.
---
According to the datasheet, there is max and min spec in the overcurrent protection trip level.
Where…
Part Number: DRV8828 For some reason the circuit attached will not result in any Ouput voltage, however I do measure 3.3V at V3P3 and Vin+10V at VCP, which I have read is correct.
We are powering the DRV with 12V (with 300uF bulk capacitance) and driving…
Part Number: DRV8828 Hi,
One of customers is using the DRV8828 to drive a printer motor. They downloaded the GUI from the software tab in the product folder.rRev B)
They ran the setup in Admin mode and the installed the required USB drivers. The COM…
Hi Yaita,
It is possible to use smaller one when you don't need high current.
You can use P=(I^2)*R. Here the I use the setting level (MAX) of DRV8828. So we can get margin with this equation.
And then, you can google the relationship of SMT…
Other Parts Discussed in Thread: DRV8828 , DRV8825 , DRV8412 , DRV8813 Hi Team, I understood DRV8828 is single H-Bridge motor driver (capable of 3A output current). Is there any dual H-Bridge stepper driver that is capable of driving up to 3A? I would…
Other Parts Discussed in Thread: DRV8828 Hi Team, My customer considers to use DRV8828(x2) for his system and see the layout of DRV8828EVM as a reference. It seems DRV8828 is far from another one, so he wants to know if it is possible to put DRV8828 closer…
Other Parts Discussed in Thread: DRV8828 , DRV8834 , DRV8824 , DRV8825 , DRV8813 , DRV8812 , DRV8829 Hi there,
We are using two DRV8828 drivers to control a 2 phase stepper motor connected to a ball screw in order to achieve some sort of linear motion…
Part Number: DRV8870 Other Parts Discussed in Thread: DRV8424E , DRV8828 , DRV8829 , DRV8436E Tool/software: Hello,
We using DRV8870 driver web tensioning application.
In this application we we driving motor in reverse direction and externally it…
Part Number: DRV8801 Other Parts Discussed in Thread: DRV8828 , Hi Team,
Our customer is looking for an H-Bridge motor driver for a 12V, 0.5A BLDC water pump motor. I have attached the details of the pump below. Upon checking our product lines, the…