Hi Matt,
The DRV8881 says that its xVREF pins are accurate down to 0.3 V.
I just noticed in your original post that you said you want to control motor speed using VREF. I'm not sure that will work. Motor speed is typically a function of the voltage…
Andrew,
Our standard reliability data is available on our website at the link below. Scroll down to "Quality & Environmental Data" heading and click on the "View" button for the package option you are interested in.
We recently released an automotive…
Hi Subbaraju,
2) Is there any IC with pmw generation with driver IC for brushed DC motor application?
What are your voltage and current requirements?
Are you looking for something like the DRV8832? Please use the DRV8832 as a starting point…
Part Number: DRV8873 Other Parts Discussed in Thread: DRV8832 , DRV8412 , DRV8702-Q1 , DRV8703-Q1 Hi Sir
AS we know,the DRV8832 can use in TEC application, may we know if DRV8873 also can use in TEC application?
if yes, may we have reference design…
Part Number: DRV8832 Other Parts Discussed in Thread: DRV8835 , DRV8837 , DRV8838 , DRV8850 , DRV8872-Q1 , DRV8837C , DRV8872 , DRV8833C , DRV8833 , DRV8848 , DRV8312
Hello,
i am new to motor control circuit and i am looking for a low voltage motor…
Part Number: DRV8842 Other Parts Discussed in Thread: DRV8832 , DRV8830
Hi Team,
The customer is using DRV8842. When OCP occurs, the nFAULT outputs a low level. The customer would like to use this low level signal as a detection
signal in his design…
Hi Kato-san,
Q1. Operation below 2V If VM voltage is below 2V, does it mean that DRV8835 cannot detect the overcurrent event ? Or does it mean that DRV8835 causes a malfunction at overcurrent event ? Which is that ? I think that the former is correct…
Hi,
wayne lu1 said:
Although I still need to use power line to transmit the data about the motor's speed or something else to control the motor.
So, do I need to buy a new device or any software I can use?
if you wish implement motor control…