Part Number: DRV8833 Hi,
I'm seeing `nFAULT` behave in a way I can't reconcile with the datasheet's documented fault conditions, on a PCB using two DRV8833 (PWP/TSSOP-16) driving three small DC motors. I'd appreciate a sanity check on whether this…
Part Number: DRV8833 Other Parts Discussed in Thread: DRV8871 , , DRV8424E , DRV8835 Hello,
I'm designing a prosthetic hand with 5 DC motors that requires independent speed and direction control for each motor. My MCU has limited PWM outputs, so I cannot…
Part Number: DRV8833 Other Parts Discussed in Thread: DRV8434-Q1 Tool/software: HI Team,
do we have plan for DRV8833 auto version?
my customer like DRV8833 hardware 4 wire PWM control. And they are asking do we have similar products in auto grade…
Part Number: DRV8833 Other Parts Discussed in Thread: DRV8210 , DRV8212 , DRV8837 Tool/software: Hello Team,
Is the DRV8833 Motor Driver Suitable for a 4V Planetary DC Gear Motor with the Following Characteristics:
No-load Current: 0.25A
Maximum…
Part Number: DRV8833 Tool/software: Hi, what is the distribution of the +/-20% error in the current regulation? Is it also dependent on temperature or just sample size?
If I have set R = 0.1 ohm then I can have 1.6A min or 2.4A max. But 2.4A overlap…
Part Number: DRV8833 Tool/software: Hi,
For the current regulation the min value is stated to 160mV and the OCP to 2A. I assume these function has random behaviour against each other for a bigger sample size. So its unlikely that one device has both…
Part Number: DRV8411 Other Parts Discussed in Thread: DRV8833 , Tool/software: Hi Team,
The customer is currently using DRV8833 on the Novatek platform (IP CAM). If he wants to use DRV8411, can the driver be directly transferred?
Part Number: DRV8833 Other Parts Discussed in Thread: DRV8231 Tool/software: Dear Team,
I hope this email finds you well. I am currently searching for a motor driver IC (or logic-level converter) with the following pin configuration:
Enable (connected…
Part Number: DRV8833
Trying to work on the project presented in Ti bulletin tiduah5 and I don't see any labels in the diagrams or photos for output pins of the DRV8833 except a problematic color coded wire with no legend. What does one do if they use…
Part Number: DRV8833 Other Parts Discussed in Thread: DRV8424 Hello,
I am using DRV8833 for a lens controlling application, is it possible to use the same H bridge driver using a regular digital signal instead pf PWM? And if not how can we use all the…