Other Parts Discussed in Thread: DRV8836EVM I have a problem with the DRV8836EVM. When I connect a motor, the EVM supplies a max of 800mA. If I connect my motor directly to the 3V power supply, the motor draws the full 1.5A specified for my motor.
Interestingly…
Other Parts Discussed in Thread: DRV8833 , DRV8836 , DRV8836EVM , DRV8839 Hi,
I am using DRV8833 as LED switching using PWM. My test input is PWM which runs with 20% duty cycle and 250hz to 1khz. I used this pulse as an input-1 for DRV8833. Then the output…