Part Number: DRV8837 Other Parts Discussed in Thread: DRV8838 Hi team,
Does DRV8837 have installed dead-time control in brake mode ? It seems to cause a short circuit by putting high levels into both IN1 and IN2
Thank you!
Part Number: DRV8837 PIN.7 is nSLEEP.Logic low puts the device in low-power sleep mode,but we need GPIO to control nSLEEP. We don't have any extra GPIO to use. Is there any other way to enter sleep mode?For example, IN1 and IN2 are logic low at the same…
Part Number: DRV8837 Hi,
I have connected nSLEEP, IN1, IN2 to the controller GPIO's. Everything is working fine but when I check the current that my circuit draws when nSLEEP = 0, it shows 1.1mA (exclusive of other peripherals on board). The datasheet…
Part Number: DRV8837 Hi E2E
We have a product that uses a DRV8837 (part marking looks like "837 OAI CHJF") to control a DC motor.
I've taken over the project and am trying to understand how the motor control was implemented.
The data sheet says…
Part Number: DRV8837 Engineering: Design a valve drive for a gas meter by using the drive chip DRV8837.
Issue: no output on the control side, but there are waveforms on both ends of the chip-to-motor, as the figure below shows:
The customer would…
Part Number: DRV8837 Hi Team,
When rotate the motor by hand, the voltage of DRV8837 VM is higher than 12V. Will it damage the device? Any way to avoid it? Thanks.
Part Number: DRV8837
Hello,
We currently use the DRV8837 in the following manner : it is a secondary low-voltage driver for a high-power torque motor. Its purpose is to allow a finer control of the motor current, when the torque needed is low. The…
Part Number: DRV8837 Dear TI Experts~
Please help me check the impact of altitude on the DRV8837 chip. Can the DRV8837 work normally at an altitude of 3000-4000 meters? The product is a E-lock
Thanks, Robin
Part Number: DRV8837 Hello,
Is it required to connect a varistor or birectional TVS diode in parallel to motor for protection against high voltage spikes? or does the IC provides protection against inductor current?
Part Number: DRV8837 Hi team,
Customer is now using magnetic encoder for rotor speed control, but now they don't want to use this any more for the cost. So, they are asking whether do we have other method to measure the speed? For example, the current…